I received the 5.8 GHz motion sensor MW0582TR11 and see there’s an LED and the serial port shows “LIGHT: 0”. Neither the datasheet or test tool describes the LED function. Is the purpose of the LED to be an ambient light sensor or light up when motion is detected? Is there an AT command to control the LED?