MCP251xFD Install issue with Jetson Nano

I have a couple MCP2518FD and MCP2517FD controller boards including the 2 CH HAT for Raspberry Pi and Jetson Nano, however following the setup guide, it does not work; 2 Channel CAN BUS FD Shield for Raspberry Pi | Seeed Studio Wiki

I follow the process and get to the point of running this command;
sudo /opt/nvidia/jetson-io/config-by-hardware.py -n “Seeed 2xMCP2518FD”
and i get the name error that “No configuration found for Seeed 2xMCP2518FD on Jetson Nano 40pin Header!”.

I am not using an emmc nano, so I thought that this process can be done via the nano module itself. Any support is appreciated.