mbed drive can not detect.

I use Arch Pro.

I connect it to Windows PC via Debug USB port with pressing Button, It can detect as “MBED LOADER” Drive.

But I connect it without pressing the button, it can not detect either “MBED LOADER” drive and “MBED” drive.



How to detect it as “MBED” Drive?

Hi there,



Connect the USB interface (next to ‘BUTTON’) of Arch Pro to your PC using a USB Micro B cable; It automatically appears as a USB device named MBED. thanks.

Hi bill.yu



I connected the USB interface (next to ‘BUTTON’) of Arch Pro to your PC using a USB Micro B cable. But, it doesn’t appears as a USB device named MBED.



Arch Pro is quiet new board. I bought it yesterday, and I just connect it once.

Only first time, the MBED drive appered.



Thanks.

I also checked on OSX and it still does not work.

Same behavior.

Hi there~,



Please make sure the usb cable is 4 wires. thanks.