LTE CAT1 hat (Europe version)

Hi,

I’m trying to install your LTE CAT1 hat (Europe version), but without success so far. I used the install-procedure as mentioned in the Wiki. Everything went OK, but the response is different, see attached picture. Questions:

  • Why is the modem not waking up?
  • Do you have any documentation on the library used to control the modem?

    Regards,

    Felix




Hi Felix



Do you go through below 4 steps? I went through the process again. I get the response from board as below. Maybe you can connect the module to windows pc to test the AT command separately to see if it works. Here is the instructions. http://wiki.seeedstudio.com/LTE_Cat_1_Pi_HAT/#faq. thanks.

-------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Software¶

Step 1. Use dtoverlay=pi3-disable-bt to enable Raspberry Pi3 UART0.



sudo nano /boot/config.txt

Then add dtoverlay=pi3-disable-bt to bottom of the config.txt



Step 2. Disable the system serivce to use the UART0.



sudo systemctl disable hciuart

Note



Pi3-disable-bt disables the Bluetooth device and restores UART0/ttyAMA0 to GPIOs 14 and 15. It is also necessary to disable the system service that initialises the modem so it doesn’t use the UART: sudo systemctl disable hciuart.



Step 3. Delete the console=serial0,115200 in cmdline.txt.



sudo nano /boot/cmdline.txt

Then delete console=serial0,115200 from the string.



Step 4. Reboot the Raspberry Pi3



sudo reboot



-------------------------------------------------------------------------------------------------------------------------------------------------------------------------

pi@raspberrypi:~ $ git clone <LINK_TEXT text=“https://github.com/Seeed-Studio/ublox_l … pi_hat.git”>https://github.com/Seeed-Studio/ublox_lara_r2_pi_hat.git</LINK_TEXT>

Cloning into ‘ublox_lara_r2_pi_hat’…

remote: Counting objects: 60, done.

remote: Total 60 (delta 0), reused 0 (delta 0), pack-reused 60

Unpacking objects: 100% (60/60), done.

pi@raspberrypi:~ $ cd ublox_lara_r2_pi_hat

pi@raspberrypi:~/ublox_lara_r2_pi_hat $ sudo python setup.py install

running install

running bdist_egg

running egg_info

creating ublox_lara_r2.egg-info

writing requirements to ublox_lara_r2.egg-info/requires.txt

writing ublox_lara_r2.egg-info/PKG-INFO

writing top-level names to ublox_lara_r2.egg-info/top_level.txt

writing dependency_links to ublox_lara_r2.egg-info/dependency_links.txt

writing manifest file ‘ublox_lara_r2.egg-info/SOURCES.txt’

reading manifest file ‘ublox_lara_r2.egg-info/SOURCES.txt’

writing manifest file ‘ublox_lara_r2.egg-info/SOURCES.txt’

installing library code to build/bdist.linux-armv7l/egg

running install_lib

running build_py

creating build

creating build/lib.linux-armv7l-2.7

creating build/lib.linux-armv7l-2.7/ublox_lara_r2

copying ublox_lara_r2/init.py -> build/lib.linux-armv7l-2.7/ublox_lara_r2

copying ublox_lara_r2/ublox_lara_r2.py -> build/lib.linux-armv7l-2.7/ublox_lara_r2

creating build/bdist.linux-armv7l

creating build/bdist.linux-armv7l/egg

creating build/bdist.linux-armv7l/egg/ublox_lara_r2

copying build/lib.linux-armv7l-2.7/ublox_lara_r2/init.py -> build/bdist.linux-armv7l/egg/ublox_lara_r2

copying build/lib.linux-armv7l-2.7/ublox_lara_r2/ublox_lara_r2.py -> build/bdist.linux-armv7l/egg/ublox_lara_r2

byte-compiling build/bdist.linux-armv7l/egg/ublox_lara_r2/init.py to init.pyc

byte-compiling build/bdist.linux-armv7l/egg/ublox_lara_r2/ublox_lara_r2.py to ublox_lara_r2.pyc

creating build/bdist.linux-armv7l/egg/EGG-INFO

installing scripts to build/bdist.linux-armv7l/egg/EGG-INFO/scripts

running install_scripts

running build_scripts

creating build/scripts-2.7

copying bin/rpirtscts -> build/scripts-2.7

creating build/bdist.linux-armv7l/egg/EGG-INFO/scripts

copying build/scripts-2.7/rpirtscts -> build/bdist.linux-armv7l/egg/EGG-INFO/scripts

changing mode of build/bdist.linux-armv7l/egg/EGG-INFO/scripts/rpirtscts to 755

copying ublox_lara_r2.egg-info/PKG-INFO -> build/bdist.linux-armv7l/egg/EGG-INFO

copying ublox_lara_r2.egg-info/SOURCES.txt -> build/bdist.linux-armv7l/egg/EGG-INFO

copying ublox_lara_r2.egg-info/dependency_links.txt -> build/bdist.linux-armv7l/egg/EGG-INFO

copying ublox_lara_r2.egg-info/requires.txt -> build/bdist.linux-armv7l/egg/EGG-INFO

copying ublox_lara_r2.egg-info/top_level.txt -> build/bdist.linux-armv7l/egg/EGG-INFO

zip_safe flag not set; analyzing archive contents…

creating dist

creating ‘dist/ublox_lara_r2-0.0.1-py2.7.egg’ and adding ‘build/bdist.linux-armv7l/egg’ to it

removing ‘build/bdist.linux-armv7l/egg’ (and everything under it)

Processing ublox_lara_r2-0.0.1-py2.7.egg

Copying ublox_lara_r2-0.0.1-py2.7.egg to /usr/local/lib/python2.7/dist-packages

Adding ublox-lara-r2 0.0.1 to easy-install.pth file

Installing rpirtscts script to /usr/local/bin



Installed /usr/local/lib/python2.7/dist-packages/ublox_lara_r2-0.0.1-py2.7.egg

Processing dependencies for ublox-lara-r2==0.0.1

Searching for pyserial==3.2.1

Best match: pyserial 3.2.1

Adding pyserial 3.2.1 to easy-install.pth file



Using /usr/lib/python2.7/dist-packages

Finished processing dependencies for ublox-lara-r2==0.0.1

pi@raspberrypi:~/ublox_lara_r2_pi_hat $ cd test

pi@raspberrypi:~/ublox_lara_r2_pi_hat/test $ sudo python test01.py

assuming 40-pin GPIO header

Enabling CTS0 and RTS0 on GPIOs 16 and 17

rts cts on

waking up… …





module name: LARA-R211

RSSI: 99

pi@raspberrypi:~/ublox_lara_r2_pi_hat/test $



Bill

Thanks, Bill! That was very helpful.

Hi,

everything with installation worked almost first time - good!

Modem works, is booked into the LTE network, reasonable RSSI.





Now - do I actually get a network device? How do I use the LTE IP-uplink?



ip a shows only the lo, eth0 and wlan0…



Thanks,

Dieter

Hi there,



please take a look at <LINK_TEXT text=“https://www.u-blox.com/sites/default/fi … 820%29.pdf”>https://www.u-blox.com/sites/default/files/AT-CommandsExamples_AppNote_(UBX-13001820).pdf</LINK_TEXT> thanks.

Hello,



I have the similar issue as Rafal. I have the European version of the U-blox Lara R211 and when trying to connect it with RPi 2 model B according to the manual, I only receive the ‘infinite’ waking up.

I successfully managed to connect to the Telekom’s LTE network and to ping google with the help of Windows and the M-Center though, so the LTE device is operational.



My questions might be somewhat dumb, but I just wanna make sure that I am doing everything right:

  1. In the wiki manual, it is not specifically stated how do you guys connect the LTE module to the RPi. Do you imply connection via USB or UART?
  2. When I connected to the Telekom’s LTE network via M-Center and Windows, I used the Telekom’s Sim-Card and it had a Pin-Code, which I had to input to the GUI in order to access the network. Could it be the reason why Rpi cannot wake the modem up?
  3. So, as I mentioned before, I have the RPi 2 Model B V1.1. However, the demo was performed at RPi 3 Model B. Could it be a compatibility issue somehow?



    Thanks beforehand for any advice!



    Cheers,

    Gleb