Is there a way for my Arduino sketch to tell when the battery attached to the LiPo Rider Pro is low or too low to continue? Will the LiPo Rider Pro stop powering my Arduino when the battery is too low for safe use?
Thank you
Is there a way for my Arduino sketch to tell when the battery attached to the LiPo Rider Pro is low or too low to continue? Will the LiPo Rider Pro stop powering my Arduino when the battery is too low for safe use?
Thank you
Hello,
You can use an Arduino analog pin to monitor the voltage of Li-po battery.
Battery capacity VS voltage:
100%----4.20V
90%-----4.06V
80%-----3.98V
70%-----3.92V
60%-----3.87V
50%-----3.82V
40%-----3.79V
30%-----3.77V
20%-----3.74V
10%-----3.68V
5%------3.45V
0%------3.00V
Hope these can help you.