Hello, I’m using UART1 for receiving the data to the LoRa E5 module and send the data through the radio. It worked fine for the baud rate 115200. When I change the baudrate from 115200 to 921600, No data is getting detected by LoRa E5 for transmission through the Radio. Clock of the peripheral is running at the 48 MHz. Is there any configuration, we need to change for 921600 baudrate or it’s the hardware limitation?
Hi there,
I believe it to be limited, to 115200. IMO.
all testing I have done the max was 115200 ![]()
HTH
GL
PJ ![]()
1 Like
it is not necessary to max out the baud rate… what da?
1 Like