Lora-E5 Development Kit and FreeRTOS AT Error while Debug

Hi,

i want to flash the FreeRTOS_LoRaWAN_AT to the Dev board. But while following the Step by Step Tutorial i get 24 Errors while debugging:

Description	Resource	Path	Location	Type
./Core/Src/adc_if.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/app_freertos.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/dma.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/main.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/rtc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/stm32_lpm_if.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/stm32wlxx_hal_msp.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/stm32wlxx_it.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/subghz.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/sys_app.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/sys_debug.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/timer_if.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/usart_if.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Core/Src/usart.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./LoRaWAN/App/lora_app.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./LoRaWAN/App/lora_at.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./LoRaWAN/App/lora_command.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./LoRaWAN/App/test_rf.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./LoRaWAN/Target/radio_board_if.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Middlewares/LoRaWAN/LmHandler/Packages/LmhpFirmwareManagement.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Middlewares/SubGHz_Phy/stm32_radio_driver/radio_driver.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Middlewares/SubGHz_Phy/stm32_radio_driver/radio_fw.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
./Middlewares/SubGHz_Phy/stm32_radio_driver/radio.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: multiple definition of `hlptim1'; ./Core/Src/adc.o:D:/Projekte/LoRaWan-E5-Node-qian/Projects/Applications/FreeRTOS/FreeRTOS_LoRaWAN_AT/Debug/../Core/Inc/main.h:102: first defined here	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem
make: *** [makefile:83: FreeRTOS_LoRaWAN_AT.elf] Error 1	FreeRTOS_LoRaWAN_AT		 	C/C++ Problem

I can flash the LoRaWAN_End_Node Project just fine but everything with FreeRTOS just gives me the same Error. Do you guys have any idea? My google searches did not guide me to a solution for this.

Thanks!

Downgraded to STM32CubeIDE 1.8.0 now it is working. Wont work with 1.9 at least for me.

1 Like

There are is in main.h and main.c somthing declared double the LPTIM_HandleTypeDef hlptim1. The right declaration is:

in main.h:

extern LPTIM_HandleTypeDef hlptim1 ;

in main.c:

LPTIM_HandleTypeDef hlptim1;

I don’t know how it was but thats the way I fixed the problem

1 Like

In main.c (or whatever the main source file is), add:

LPTIM_HandleTypeDef hlptim1;

without extern.