Hello,
I have a seeeduino 4.2 board, and a grove LoRa-E5 module that I wanted to use for LoRa communication, however the example code doesn’t work.
The code is on this page :
The errors I get are :
‘Serial1’ was not declared in this scope
By adding  “#include <SoftwareSerial.h>”
and  “SoftwareSerial Serial1(10, 11); // RX, TX” the error changes to :
class SoftwareSerial’ has no member named ‘printf’; did you mean ‘print’?
Can someone help me on this please?
Thank you!