Hello
Sorry, but I do not speak English very well. I apologized for the bad sentence.
I wanted to know if I can recharge the battery with lipo rider pro because the battery is cilyndric. I do not think it bothers, but I prefer to be on. It has a large capacity and can go into a base.
I can not put a link, but on the internet it is possible to end up with these instructions:
UltraFire 18650 3.7V 3000mAh Rechargeable Battery
Is that I could put 2 new batteries / /
thank you