LiPo Rider Plus Faulty?

I currently use three LiPo Rider Plus boards inside small acquisition modules.
Aside from the annoying fact that when the USB-C port loses power, the 5V output turns off and then on, with about a seconds delay. I have now noticed that with only the battery connected, with and without load, the 5V out dips from 4.9V to 3.7V every second or so. Does this indicate a faulty module?
I’m hesitant to disassemble the remaining two modules to test the other LiPo RIder Plus boards.
Any insight may help.

@nino.benci Yes, you’re right. Here is the waveform of power plug in and pull out.


Maybe we can talk about the next generation of lipo rider?

Hi Bruce.

Happy to chat.

The current version is a power bank solution. The original intention of the design is a small power board with typec and typeA interface. Since TyeC is popular now, many users use C-C line, so our type C port needs to have the current output function. The same port as input and output will cause the main controller to shut down the output for a while when switching functions. We are looking for a suitable solution. What suggestions do you have?

Hijacking this thread with a response.

The Lipo Rider Plus should have the following bare minimum requirements:

  • Boost voltage (not just pass through power) from USB source to 5.1 V to recover voltage lost from long USB cables and support Raspberry Pi and other devices that require >5.0 V.

  • Switching between battery and USB power without loss of power. This should be possible if boosting both sources, rather than just battery. Refer to PowerBoost 1000C by Adafruit as an example.

  • JST connector should be moved/rotated to not be on the same side as the USB-C port. This will allow the module to be put inside a case with an internal battery, but external USB-C connection.

Hi All,

Sorry to hijack this thread, but given that i can’t create new topics and the title of this one is rather broad, i thought i’d give it a shot.

I recently purchased the Lipo Rider Plus and was expecting that the USB-A to USB-C port would be pass-through. I didn’t really read anything contradicting this in the product description(s).

Is this board designed with USB pass-through in mind, or only for charging Lipo batteries and powering devices? (I wasn’t really able to figure it out on the schematics) - or did I ruin the pass-through with my tinkering?

Many thanks in advance!

Herman

Hi there,

And Welcome Here…

So , Short answer “NO” … NOT at all, Not even a little.

Its a battery charger with some tricks is all really, meant for the solar power and Battery charge arena’s But thanks :hand_with_fingers_splayed: for the contribush
:grin:

HTH
GL :slight_smile: PJ :v:

Thx a lot for your reply @PJ_Glasso ! Guess I was a bit optimistic there :smiley:

Just out of curiousity, do you think it would be possible to break out the D+/D- pins on the USB-C? I think it’s doable on the USB-A side, but the USB-C side the connections are very tiny… it’s not really clear on the PCB layout if it would be possible though.

Feel free to share your 2 cents on this one!

Thx,

H

Hi there,

So on the schematic , you can use it “unconventionally” but any Smoke , you’ll need to own :grin:
As long as you don’t exceed the power draw of the supply /2 , then you can use the terminal as a form of a 12v splitter , Barrel jack would be input, terminal block is now parrallel with that but unfused :backhand_index_pointing_left: :wink:
You can connect to it, but DO not exceed the current draw from the Driver board and what ever string of LED’s you use. (check your total (i))
It’s NOT brain :brain: Surgery but measure everything so to keep it safe :+1:
Follow along with the schematic. It’s a solid little board and can’t beat the Price vs. features SO , LED the WAY

HTH
GL :slight_smile: PJ :v: