Looking at the lipo rider with the output usb port down and the solar and battery ones up we can see that the + pin of these two ports are on the right and the - on the left. But If we look at photos on the wiki site the the red cable of the battery goes on left pin and the black on the right!
I have bought a battery pack with a JST 2mm pin and it fits in the same way of seedstudio photos. So, before connect pins on the wrong way and damage everything I ask: is it possible that pins on lipo rider are wrongly labeled?
Thanks in advance
The pins on lipo rider board is right . the picture on the wiki is different in previous versions .