LinkitOne power consumption

Deat tech team,



We are about to use this ready product for a Project that will be used in vehicles. That is why I would like to learn the average power consumption values(current consumption at 3.7V) when;


  • GPS is active
  • GPRS is connected
  • BLE is active

Hi

Erman


We do not have the data on hand, We can setup and run code with different situations. It will take some time. Keep you posted.

Thanks

best rgds
Bill

Dear Bill,



That would be great. Also we would be glad to know whether we can take the module into low power or sleep modes whenever needed.

Hello,



Thank you for waiting. Now the power of the circuit board was measured. Here is the result:

- GPRS is active
During standby time, the power consumption of the board is 0.02a*3.7v.
When there is a call, the power consumption of the board can be up to 0.15a*3.7v.

- GPS is connected
During the most time, the power consumption of the board is 0.05a*3.7v.
In some moments, the power consumption of the board can be up to 0.15a*3.7v.

- BLE is active
During the most time, the power consumption is about 0.05a*3.7v, but it can be up to 0.12a*3.7v when the connection is active.

Thanks

best rgds
Mancy