Yeah that makes sense. I’ve been basically doing that for 8 months and have kind of topped out at about 1mA in deep sleep on an MG24. The two things I need are the IMU (only when awake as I don’t need it to wake the device) and flash storage (using the EEPROM library that comes with silabs). I’m about ready to throw in the towel and say that’s the lowest it can go - so maybe what I’m looking for is a gut check - does that number seem about right for having to use those two things?
1 Like