Welcome! Please be Moderated!
Wow, you did it !
We are struggling to wake up MG24 with GPIO wake from EM4 deep sleep but without any luck. I was wondering if you could share the bit of the code with the sleeping and waking from EM4 when GPIO is triggered. Thanks
Hi there,
And Welcome here…
So , If I may we like to keep things tidy and easy to find here. Allow me to demonstrate just how easy it is to find the answers using the search and a picture. Once you get a few posts , reply’s or questions to get enough forum Cred to post a NEW topic , a PIC/VIDeO or your own Question.
HTH
BTW there are some very good code examples he has in these threads listed… ![]()
GL
PJ ![]()
@bigpil - I am away from the office right now but have you looked at the Low Power Example for the MG24?
Thak you for the link. We managed to get down to 37.4uA without timed wake up or GPIO wake. If we add these, the current goes close to 1mA. Any suggestion on how to get a lower current ?
I was trying to add a picture with the code but I am getting an error.
Which version of XIAO MG24 are you using? With Sense?
I’ll post my code later today.
Unfortunately was busy today (Saturday) so code will have to wait until Monday.
I am using MG24 from here : Seeed XIAO MG24 | The Pi Hut
I am basically trying to make an audio device where an MG24 will go to deep sleep mode, and when it wakes up, it powers up a mini df-player via a mosfet and sends instructions on what files to play first according to the GPIO . We are bassicaly trying to build an ultra low power audio unit right now, but I am planning to use it for other projects as well. The whole unit will run on 3x AAA batteries. We are testing the deep sleep mode current at the moment without any other code.
This is the code we are using right now for testing.
#include <Arduino.h>
#include "ArduinoLowPower.h" // Arduino Low Power Library
void setup() {
//Serial.begin(115200);
}
void loop() {
//Serial.println(F("Hello..."));
delay(10000);
//Serial.println(F("Entering sleep mode..."));
LowPower.deepSleep(); // go to deep sleep
}
Thanks for the extra information. What is being used to do the actual wake up? Is is a push button or a toggle switch or something else?
There is quite a bit of extra support code required for initial setup of deep sleep mode.
Will you be using the radio at all?
Hi, yes, it will be a momentary push button.
In that case I suggest a simple pull up resistor on the button. I tested with 220k and it worked fine, current was < 1.8uA in Deep Sleep.
The code and test drawing is here.
If you want to use basic code and still have < 2uA current consumption, it can be done with the standard XIAO Deep Sleep example and using GPIO and Timed wakeup.
Another option I use on keyfob remotes is to use the push button to latch the power on. That requires additional circuitry but uses zero power.
Thanks for the picture
Glad you got it working!
For a Fob (3V battery), I just use a switch to power the device. In your case (~4.5V battery) you can use a P-Ch Mosfet for power and switched with an N-Ch Mosfet for switching the power.
A simple circuit is below.
Switch turns on the power, Hold (GPIO) keeps it turned on until no longer required.
Thanks, it look sinteresting, I’ll give it a try this week. Any idea what is the waking-up time and how quick the script can run ?
In all of these low power examples, I see the flash commands and functions - what do they do and how do they relate to low power? I’m assuming they turn something off, but it is unclear.
edit:
Ok the code issues a deep power down command to the flash storage I gather. But what if I want flash storage? And the IMU for that matter? Is it impossible to achieve these low power rates if you want to use those things?
Hi there,
So the threads you reference are ALL towards the lowest sleep current.
You can do many,many things to use the flash and IMU and still save power, but it up to you to determine which tech ,bsp’, flash sleep, bootloader ,system ON sleep ,etc.is right for your project.
There isn’t a how to on the customized power profiles, you will need to test and measure and reprogram accordingly. Lots of smart folks with experience with the nuance of it. So ask about specific needs and see what comes back
HTH
GL
PJ ![]()
Using a combination of methods helped me save Mah of battery so try everything
Yeah that makes sense. I’ve been basically doing that for 8 months and have kind of topped out at about 1mA in deep sleep on an MG24. The two things I need are the IMU (only when awake as I don’t need it to wake the device) and flash storage (using the EEPROM library that comes with silabs). I’m about ready to throw in the towel and say that’s the lowest it can go - so maybe what I’m looking for is a gut check - does that number seem about right for having to use those two things?
Both nRF52840 and MG24 allow you to turn the IMU on and off, and the flash has power-down and wake-up commands.
Turning off the IMU, powering down the flash, and then putting XIAO into sleep mode will give you the best sleep current. Wake up XIAO, turn on the IMU, and wake up the flash, and you can use it however you like.
If you can provide specific details about your issue, many people will be able to assist you.
The post #35 in the link below may be helpful.