I have a couple new LHT65s and a the things indoor gateway (TTIG)
I think I have the gateway setup correctly it appears in “the things stack” as connected. When I hold down the ACT button on the LHT65 for 5 seconds it blinks green 5 times then red and that is it on the unit? on the the things stack webpage I see a msg in the live data that it "Received uplink message : JoineEUI :### DevEUI:### bandwith 125000 …: and the msg continues to a raw payload string of #products:shields
So I have a couple of questions
- shouldn’t the LHT65 have a green light blink at the end of holding down the act button?
- does the LHT65 have to be identified in an app as an end device for this to happen?
- I created a blank app and added the end device and i see data when I hit the act button but it does not appear to be automatic?
is there a good demo/tutorial someone can recommend
Thanks
Tball