LED Bar and Teensy 4.1

Controlling a LED Bar using a Teensy 4.1 doesn’t seem to be working, even though there’s no problem when using an UNO R3 clone with the same test sketch.
Is there a solution ?
Thanks

Hi there,

So ,
Are you sure, it’s a 3.3v device or a 5V device…

HTH
GL :slight_smile: PJ :v:

Here is the excellent solution provided by Paul Stoffregen on the PJRC forum: reduce the CPU speed to 24 MHz

https://forum.pjrc.com/index.php?threads/grove-led-bar-teensy-4-1.77864/post-367609