I get an increase in jitter on a connected joystick when I plug in a USB cable and start charging the battery.
The increased jitters go away once the battery is fully charged.
The device I’m inventing is a buttons and a joystick over wifi affair. The joystick had natural jitter, so I spent a lot of time with the sketch trying to suppress its effect so it wouldn’t send commands to the receiver when it was centered and nobody was touching it. I did that with it connected to my computer with a USB cable using serial monitor on Arduino IDE to get the raw numbers. Eventually, I had it mostly stable. Output to serial monitor was silent. Maybe there was a long spike every once in a while that got past the sample rate, but it was rare.
Then, I plugged in a battery. The jitters came back. Or, they were just increased past the dampening settings I established. I know, because serial monitor says so, but also because the LED I added to show transmissions flashes. The effect happens also when I’m connected to a wall charger. Not just when connected to computer. I only started having this problem when I switched to the seeed board because of the on-board charging to reduce size. I was using an external battery charging circuit with a different board before.
The effect happened with a 250 mah battery and a 2000 mah battery and on two separate builds of the device using different boards in each.
Here is the way I have it wired:
D0 button
D1 button
D2 VRY
D3 button
D4 packet sending LED
D5 button
D6 button
D7 wifi is connected LED
0.1 uf capacitor across GND and +5V on the joystick
220 nf capacitor across GND and D2 on the board
330 ohm resistor between VRY on the joystick and D2 on the board
330 ohm resistors between the pins and each LED
+5V on the joystick is wired to 3V3 from the board
The joystick is a generic mushroom cap thumb type you can get from amazon postings that say “blah blah for arduino blah blah” on all the listings.
Is this a known issue? My search of the forums didn’t find anything. How can I fix it?
Sounds like a cool project, and I think it’s been on here before, A thumb version with BLE, not wifi. So for prior art , your covered
The battery charger is noisy perhaps the draw on it is too high. You look to have a pretty beefy battery with high charge current req’s,
I would try to manage that better, stay with the smaller one, work with that until it is solved. add a big Supply bypass cap , close the the +vcc pin and GND, the WIFI is a power hog, and a transient maker..on the C3, and where is your antenna at? try one of the larger stub versions also, you may be surprised with the results.
Post up a picture of this amazing Apparatus, lots of smart folks on here willing to help.
and definitely watch those resistor values.
my first glance , recommends.
I think this must be a V Ref issue… but i dont know how to fix it.. unless using an ADC pin to run a caliberation map… maybe a capacitor on the power side of the sensor… IMO
There’s only one ground pin for it to go to. There’s a gnd pad on the bottom, but I’m only using that for an on/off switch. Are people getting joystick jitters from usb charging due to separate grounds? I don’t see how separate grounds is possible.
… i think what he is saying is jitter can sometimes be caused by a ground fault or loose connection, most often breadboard where the current birst will cause buildup of resistance and heat… FYI
@wacad, reading through the thread, the useful clue is that adding 10 uF across 3V3 and GND reduced the jitter. That suggests supply noise or transients were contributing, although it doesn’t pinpoint the source.
On the grounding question, your wiring description already indicates a common ground. The remaining consideration is the physical return path: wires and contacts have resistance and inductance, so changing currents can produce small voltage differences even between connected ground points. Analog Devices explains this effect here.
I noticed you already have 330 ohm in series with VRY and 220 nF between D2 and GND. That provides input filtering; I’d check that the capacitor sits close to D2 with a short ground connection. This is consistent with Espressif’s ESP32-C3 ADC noise guidance, which recommends an input capacitor and multisampling.
If you’re moving the design onto a PCB, keeping the decoupling connections short will help preserve the improvement you found. This capacitor-placement guide covers the layout considerations.
With the 10 uF fitted, do the raw readings now stay within roughly the same range on battery power and during active charging, or has the improvement mainly stopped the unwanted commands?