Jetson Mate Wiki setup fails when trying to intialize cluster

Hi when I try to initialize the jetson mate cluster I get the following error. Any help would be apprecited!:
[kubelet-check] The HTTP call equal to ‘curl -sSL http://localhost:10248/healthz’ failed with error: Get “http://localhost:10248/healthz”: dial tcp 127.0.0.1:10248: connect: connection refused.
[kubelet-check] It seems like the kubelet isn’t running or healthy.

I tried this.
and
Success!
It’s Docker and Kubernetes Driver problem.

sud cat < /etc/sysctl.d/k8s.conf

net.bridge.bridge-nf-call-ip6tables = 1
net.bridge.bridge-nf-call-iptables = 1
EOF
sudo sysctl --system

// Edit “/etc/docker/daemon.json”

{
“exec-opts”: [“native.cgroupdriver=systemd”],
“log-driver”: “json-file”,
“log-opts”: {
“max-size”: “100m”
},
“storage-driver”: “overlay2”,
“default-runtime” : “nvidia”,
“runtimes”: {
“nvidia”: {
“path”: “nvidia-container-runtime”,
“runtimeArgs”:
}
}
}

// Restart daemon,docker
sudo systemctl daemon-reload && sudo systemctl restart docker

//Reset kubeadm
sudo kubeadm reset

//delete files
sudo rm /var/lib/etcd
sudo rm /etc/kubernetes/manifests/kube-apiserver.yaml
sudo rm /etc/kubernetes/manifests/kube-controller-manager.yaml
sudo rm /etc/kubernetes/manifests/kube-scheduler.yaml
sudo rm /etc/kubernetes/manifests/etcd.yaml

// Init
sudo kubeadm init --pod-network-cidr=10.244.0.0/16