Can Jetson Mate be used with 4x Jetson TX2 NX?
According to Jetson Mate - Seeed Wiki Jetson Nano or Jetson NX SoMs can be used. But I’m not sure if Jetson NX also includes TX2 NX.
Can Jetson Mate be used with 4x Jetson TX2 NX?
According to Jetson Mate - Seeed Wiki Jetson Nano or Jetson NX SoMs can be used. But I’m not sure if Jetson NX also includes TX2 NX.
Update: Yes it seems to work with Jetson TX2 NX.
I was not able to use the SDKManager GUI to flash the TX2 NX. Instead, I used the following command:
cd ~/nvidia/nvidia_sdk/JetPack_4.6.2_Linux_JETSON_TX2_TARGETS/Linux_for_Tegra
sudo ./flash.sh jetson-xavier-nx-devkit-tx2-nx mmcblk0p1