Jetson AGX Orin H01 Kit, compatible with Jetpack 6.2.1 (rev1) / L4T 36.4.7?

Hi,
after my last step, flashing the device to 6.2/L4T 36.4.3 with success, i am wondering if i should upgrade to the last Nvidia release. i dont want to do something wrong as the unit is working fine.

Please, confirm that upgrading to Jetpack 6.2.1 (rev1) / L4T 36.4.7 will not break the system.
this can be done with a simple apt upgrade
…
thanks a lot :pray:

Hi there,

I would be cautious on that, I was alluding to which that has broken some systems.

I would wait until Seeed confirms. I know it sounds counterintuitive, but look at past post on other updates where users tried and bricked. or had NO video or Wifi in one case.

HTH

GL :slight_smile: PJ :v:

Thanks a lot @PJ_Glasso , i always try things with caution, and as i said my unit is working properly, so i dont want to mess things up.. you are right, lets wait Seeed confirms this last upgrade will have the necessary libs to fit their devices. i will keep the 36.4.3, until their answer.
have a great day