J3011/J401 Flashing fails - line 43: remove_udev_rules: command not found

Hi all,

Trying to flash my J3011 with JP6 using instructions from

I’m using Ubuntu 22.04.4 LTS on WSL 2

First I downloaded

Jetson_Linux_R36.3.0_aarch64.tbz2
Tegra_Linux_Sample-Root-Filesystem_R36.3.0_aarch64.tbz2

…
Could see 0955 7523 etc.
…

tar xf Jetson_Linux_R36.3.0_aarch64.tbz2
sudo tar xpf Tegra_Linux_Sample-Root-Filesystem_R36.3.0_aarch64.tbz2 -C Linux_for_Tegra/rootfs
cd Linux_for_Tegra/
sudo ./apply_binaries.sh
sudo ./tools/l4t_flash_prerequisites.sh

This seemed a bit odd as already in Linux_for_Tegra dir

sudo tools/l4t_create_default_user.sh -u MyUser -p MyPassword -a -n MyMachine --accept-license

Then ran

sudo ./tools/kernel_flash/l4t_initrd_flash.sh --external-device nvme0n1p1
-c tools/kernel_flash/flash_l4t_t234_nvme.xml -p “-c bootloader/generic/cfg/flash_t234_qspi.xml”
–showlogs --network usb0 jetson-orin-nano-devkit internal

which failed with

sudo ./tools/kernel_flash/l4t_initrd_flash.sh --external-device nvme0n1p1 -c tools/kernel_flash/flash_l4t_t234_nvme.xml -p “-c bootloader/generic/cfg/flash_t234_qspi.xml” --showlogs --network usb0 jetson-orin-nano-devkit internal
cat: /sys/module/usbcore/parameters/autosuspend: No such file or directory
./tools/kernel_flash/l4t_initrd_flash.sh: line 43: remove_udev_rules: command not found

Tried with SDK manager think same issue.

Any suggestions?

Thanks

Bryn