hi.
When I connect the J1010 to power, after the Nvidia screen appears, the original JetsonNano desktop does not appear and an error occurs.
The contents of the error are ‘Failed to start Hostname Service’, ‘Failed to start Configure USB flashing port for device mode’, ‘Failed to start Docker Application Container Engine’.
Then the desktop appears on a black screen with a few lines of text.
how do i solve it?
Hi, Nilson,
English as my second language, I describe as clearly as possible:
‘Failed to start Docker Application Container Engine’, because docker did not start, first check whether elasticsearch service exists
[root@warehouse00 ~]# docker ps|grep elastic
Cannot connect to the Docker daemon at unix:///var/run/docker.sock. Is the docker daemon running?
The docker status is failed
[root@warehouse00 ~]# service docker status
Redirecting to /bin/systemctl status docker.service
● docker.service - Docker Application Container Engine
Loaded: loaded (/etc/systemd/system/docker.service; enabled; vendor preset: disabled)
Active: failed (Result: start-limit) since Mon 2020-06-15 06:30:16 UTC; 1 weeks 1 days ago
Docs: https://docs.docker.com
Process: 19410 ExecStart=/usr/bin/dockerd -H fd:// (code=exited, status=1/FAILURE)
Main PID: 19410 (code=exited, status=1/FAILURE)
Jun 15 06:30:16 warehouse00 systemd[1]: docker.service holdoff time over, scheduling restart.
Jun 15 06:30:16 warehouse00 systemd[1]: Stopped Docker Application Container Engine.
Jun 15 06:30:16 warehouse00 systemd[1]: start request repeated too quickly for docker.service
Jun 15 06:30:16 warehouse00 systemd[1]: Failed to start Docker Application Container Engine.
Jun 15 06:30:16 warehouse00 systemd[1]: Unit docker.service entered failed state.
Jun 15 06:30:16 warehouse00 systemd[1]: docker.service failed.
Jun 15 06:30:33 warehouse00 systemd[1]: start request repeated too quickly for docker.service
Jun 15 06:30:33 warehouse00 systemd[1]: Failed to start Docker Application Container Engine.
Jun 15 06:30:33 warehouse00 systemd[1]: docker.service failed.
Jun 23 07:45:16 warehouse00 systemd[1]: Unit docker.service cannot be reloaded because it is inactive.
Start dockerd manually
[root@warehouse00 ~]# dockerd
INFO[2020-06-23T07:46:26.609656620Z] Starting up
INFO[2020-06-23T07:46:26.615956282Z] libcontainerd: started new containerd process pid=1802
INFO[2020-06-23T07:46:26.616133833Z] parsed scheme: "unix" module=grpc
INFO[2020-06-23T07:46:26.616167280Z] scheme "unix" not registered, fallback to default scheme module=grpc
INFO[2020-06-23T07:46:26.616225318Z] ccResolverWrapper: sending update to cc: {[{unix:///var/run/docker/containerd/containerd.sock 0 <nil>}] <nil>} module=grpc
INFO[2020-06-23T07:46:26.616255985Z] ClientConn switching balancer to "pick_first" module=grpc
INFO[2020-06-23T07:46:26.665833586Z] starting containerd revision=b34a5c8af56e510852c35414db4c1f4fa6172339 version=v1.2.10
INFO[2020-06-23T07:46:26.667139004Z] loading plugin "io.containerd.content.v1.content"... type=io.containerd.content.v1
INFO[2020-06-23T07:46:26.667283454Z] loading plugin "io.containerd.snapshotter.v1.btrfs"... type=io.containerd.snapshotter.v1
WARN[2020-06-23T07:46:26.667700679Z] failed to load plugin io.containerd.snapshotter.v1.btrfs error="path /var/lib/docker/containerd/daemon/io.containerd.snapshotter.v1.btrfs must be a btrfs filesystem to be used with the btrfs snapshotter"
INFO[2020-06-23T07:46:26.667751093Z] loading plugin "io.containerd.snapshotter.v1.aufs"... type=io.containerd.snapshotter.v1
WARN[2020-06-23T07:46:26.672276961Z] failed to load plugin io.containerd.snapshotter.v1.aufs error="modprobe aufs failed: "modprobe: FATAL: Module aufs not found.\n": exit status 1"
INFO[2020-06-23T07:46:26.672329642Z] loading plugin "io.containerd.snapshotter.v1.native"... type=io.containerd.snapshotter.v1
INFO[2020-06-23T07:46:26.672396890Z] loading plugin "io.containerd.snapshotter.v1.overlayfs"... type=io.containerd.snapshotter.v1
INFO[2020-06-23T07:46:26.672604691Z] loading plugin "io.containerd.snapshotter.v1.zfs"... type=io.containerd.snapshotter.v1
INFO[2020-06-23T07:46:26.673060327Z] skip loading plugin "io.containerd.snapshotter.v1.zfs"... type=io.containerd.snapshotter.v1
INFO[2020-06-23T07:46:26.673097387Z] loading plugin "io.containerd.metadata.v1.bolt"... type=io.containerd.metadata.v1
WARN[2020-06-23T07:46:26.673137831Z] could not use snapshotter btrfs in metadata plugin error="path /var/lib/docker/containerd/daemon/io.containerd.snapshotter.v1.btrfs must be a btrfs filesystem to be used with the btrfs snapshotter"
WARN[2020-06-23T07:46:26.673161222Z] could not use snapshotter aufs in metadata plugin error="modprobe aufs failed: "modprobe: FATAL: Module aufs not found.\n": exit status 1"
WARN[2020-06-23T07:46:26.673185176Z] could not use snapshotter zfs in metadata plugin error="path /var/lib/docker/containerd/daemon/io.containerd.snapshotter.v1.zfs must be a zfs filesystem to be used with the zfs snapshotter: skip plugin"
INFO[2020-06-23T07:46:26.673528926Z] loading plugin "io.containerd.differ.v1.walking"... type=io.containerd.differ.v1
INFO[2020-06-23T07:46:26.673583123Z] loading plugin "io.containerd.gc.v1.scheduler"... type=io.containerd.gc.v1
INFO[2020-06-23T07:46:26.673692715Z] loading plugin "io.containerd.service.v1.containers-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673736540Z] loading plugin "io.containerd.service.v1.content-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673769457Z] loading plugin "io.containerd.service.v1.diff-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673804631Z] loading plugin "io.containerd.service.v1.images-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673839842Z] loading plugin "io.containerd.service.v1.leases-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673903483Z] loading plugin "io.containerd.service.v1.namespaces-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673943174Z] loading plugin "io.containerd.service.v1.snapshots-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.673979791Z] loading plugin "io.containerd.runtime.v1.linux"... type=io.containerd.runtime.v1
INFO[2020-06-23T07:46:26.674145534Z] loading plugin "io.containerd.runtime.v2.task"... type=io.containerd.runtime.v2
INFO[2020-06-23T07:46:26.674279834Z] loading plugin "io.containerd.monitor.v1.cgroups"... type=io.containerd.monitor.v1
INFO[2020-06-23T07:46:26.675734289Z] loading plugin "io.containerd.service.v1.tasks-service"... type=io.containerd.service.v1
INFO[2020-06-23T07:46:26.675851914Z] loading plugin "io.containerd.internal.v1.restart"... type=io.containerd.internal.v1
INFO[2020-06-23T07:46:26.676034068Z] loading plugin "io.containerd.grpc.v1.containers"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676081089Z] loading plugin "io.containerd.grpc.v1.content"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676117009Z] loading plugin "io.containerd.grpc.v1.diff"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676149377Z] loading plugin "io.containerd.grpc.v1.events"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676180874Z] loading plugin "io.containerd.grpc.v1.healthcheck"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676214131Z] loading plugin "io.containerd.grpc.v1.images"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676245682Z] loading plugin "io.containerd.grpc.v1.leases"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676284266Z] loading plugin "io.containerd.grpc.v1.namespaces"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676316443Z] loading plugin "io.containerd.internal.v1.opt"... type=io.containerd.internal.v1
INFO[2020-06-23T07:46:26.676440092Z] loading plugin "io.containerd.grpc.v1.snapshots"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676482597Z] loading plugin "io.containerd.grpc.v1.tasks"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676514017Z] loading plugin "io.containerd.grpc.v1.version"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.676545815Z] loading plugin "io.containerd.grpc.v1.introspection"... type=io.containerd.grpc.v1
INFO[2020-06-23T07:46:26.677125349Z] serving... address="/var/run/docker/containerd/containerd-debug.sock"
INFO[2020-06-23T07:46:26.677301919Z] serving... address="/var/run/docker/containerd/containerd.sock"
INFO[2020-06-23T07:46:26.677337263Z] containerd successfully booted in 0.013476s
INFO[2020-06-23T07:46:26.693415067Z] parsed scheme: "unix" module=grpc
INFO[2020-06-23T07:46:26.693481428Z] scheme "unix" not registered, fallback to default scheme module=grpc
INFO[2020-06-23T07:46:26.693528406Z] ccResolverWrapper: sending update to cc: {[{unix:///var/run/docker/containerd/containerd.sock 0 <nil>}] <nil>} module=grpc
INFO[2020-06-23T07:46:26.693554473Z] ClientConn switching balancer to "pick_first" module=grpc
INFO[2020-06-23T07:46:26.695436116Z] parsed scheme: "unix" module=grpc
INFO[2020-06-23T07:46:26.695494014Z] scheme "unix" not registered, fallback to default scheme module=grpc
INFO[2020-06-23T07:46:26.695532298Z] ccResolverWrapper: sending update to cc: {[{unix:///var/run/docker/containerd/containerd.sock 0 <nil>}] <nil>} module=grpc
INFO[2020-06-23T07:46:26.695558869Z] ClientConn switching balancer to "pick_first" module=grpc
INFO[2020-06-23T07:46:26.747479158Z] Loading containers: start.
INFO[2020-06-23T07:46:26.887145110Z] stopping event stream following graceful shutdown error="<nil>" module=libcontainerd namespace=moby
INFO[2020-06-23T07:46:26.887630706Z] stopping healthcheck following graceful shutdown module=libcontainerd
INFO[2020-06-23T07:46:26.887672287Z] stopping event stream following graceful shutdown error="context canceled" module=libcontainerd namespace=plugins.moby
failed to start daemon: Error initializing network controller: Error creating default "bridge" network: could not find an available, non-overlapping IPv6 address pool among the defaults to assign to the network
** Inspect daemon.json**
[root@warehouse00 ~]# cat /etc/docker/daemon.json
{
"insecure-registries": ["registry.local", "127.0.0.1:5001", "10.10.13.42:5000"],
"registry-mirrors": ["http://mirror.local"],
"bip": "172.18.18.1/24",
"data-root": "/var/lib/docker",
"ipv6": true,
"storage-driver": "overlay2",
"live-restore": true,
"log-opts": {
"max-size": "500m"
}
}
Modify daemon.json
Delete the ipv6:true setting.
After daemon authentication was manually started and ipv6:true was changed, it was found that the problem was not repeated.
When docker restarts, the error message “Job for docker.service invalid” is displayed.
[root@warehouse00 ~]# systemctl reload docker
Job for docker.service invalid.
Start daemon and docker with systemctl
$ sudo systemctl start docker
$ sudo service docker start
I hope these steps will help you !
Jostar