I am interested to know if someone of you by any chance has the J101-v2 carrier board for jetson nano and was able to configure the 40pin header (spi interface) ?
I installed the dt-overlays according to https://github.com/Seeed-Studio/seeed-linux-dtoverlays to be able to use the SPI interface but when I want to manually configure the 40pin header I receive this error:
FATAL ERROR! |
| |
| |
| Failed to get pin number for node |
| /fragment@10/__overlay__/header-40pin-spi0-pinmux/pin18/! |
| |
| Press any key to terminate
I addressed my issue to their support and I received this reply which is very ambiguous to me:
This device can only be used with the official nvidia jetson nano dev kit.
Output of /opt/nvidia/jetson-io/config-by-hardware.py -l is:
Header 1 [default]: Jetson 40pin Header
Available hardware modules:
1. Seeed 2xMCP2518FD
2. reComputer sdmmc
Header 2: Jetson Nano CSI Connector
Available hardware modules:
1. Camera IMX219 Dual
2. Camera IMX477 Dual
3. Camera IMX477-A and IMX219-