Issue with wifi on Xiao ESP32S3

Hello,

We bought two ESP32S3 at work as surveillance devices for long run experiments. Unfortunately, I could not achieve a reliable behavior of the wifi during the connection process. I used the standard example but WiFi.begin(ssid, password) works only after a manual reboot of the board using the button.

What steps I took to try to pinpoint the issue :

  • Using the same program at work and at home to see if it was related to one specific access point
  • Loading the program with VisualStudio/PlatformIO at work and Arduino-CLI at home
  • Rebooting the board by turning on and off the power of the RaspberryPi3’s internal usb hub I’m using at home using uhubctl
  • Soft rebooting the board by using the resetFunc function (ressource)
  • Hard rebooting the board by emulating the reset performed by the IDE after programming the board (ressource) ; my brother cleaned the Bash/C code of the original author for me, I’ll put the new one below and we will probably implement it in Python in the near future
  • Increasing pauses (from the original 100 ms to 10 s) between WiFi.disconnect(); and WiFi.begin(ssid, password);
  • Adding a step at which we wait for any user input by checking the size of the serial input buffer to manually start the wifi connection when our serial terminal is up to be sure to miss nothing

The thing I haven’t tried for now is to wire the EN pad to a digital output in order to simulate a push of the button directly in the program and avoid pushing on it manually. I still hope to understand the issue and have a more reliable behavior.

I also haven’t tried to adapt the standard test code to use different wifi functions (WiFi.disconnect(); with wifioff or eraseap parameters, WiFi.reconnect(), or WiFi.waitForConnectResult(), etc.).

Does someone have an idea on what I am doing wrong and/or what could be the solution?

EDIT: I played a little bit with WiFi.waitForConnectResult() and WiFi.status() and according to the Arduino reference, it seems that when calling WiFi.begin(), the status should switch to WL_IDLE_STATUS. But for me it is directly on WL_DISCONNECTED: at the function return value, right after the call, or until the end of the timeout. So it seems that WiFi.begin() is not behaving as it should for me.

Many thanks in advance!

Martin.


The last iteration of the wifi init code we tried:

void init_wifi() {
  // Set WiFi to STA mode and disconnect from an AP if it was previously connected
  Serial.print("Initializing WiFi");
  WiFi.mode(WIFI_STA);
  WiFi.disconnect();
  delay(1000);
  Serial.print(".");
  Serial.println();

  // Set WiFi to STA mode and connect to AP
  Serial.print("Connecting to WiFi");
  WiFi.mode(WIFI_STA);
  WiFi.begin(ssid, password);
  delay(1000);
  Serial.print(".");
  Serial.println();
  
  // Wait for opened connection
  while (WiFi.status() != WL_CONNECTED) {
    Serial.print(".");
    delay(1000);
  }
  Serial.println();

  // Print IP address
  Serial.print("Obtained IP address: ");
  Serial.println(WiFi.localIP());
  Serial.println();
}

The code we used on the RaspberryPi to send a reset though the serial port (called with the serial port as an argument: ./ahr /dev/ttyACM0):

#include <errno.h>
#include <fcntl.h>
#include <sys/ioctl.h>
#include <stdio.h>
#include <string.h>
#include <unistd.h>
#include <stdlib.h>

int main(int argc, char* argv[]) {
  if (argc < 2) {
    fprintf(stderr, "need serial device\n");
    exit(1);
  }
  char* sport = argv[1];
  unsigned int delay = 1;

  int port_fd = open(sport, O_RDWR | O_NOCTTY);
  if (errno)
    printf("Error opening %s: %s (%d).\n", sport, strerror(errno), errno);
  int modem_ctrl, modem_ctrl_saved;
  if (ioctl(port_fd,TIOCMGET,&modem_ctrl_saved) == -1)
    printf("Error getting handshake lines: %s (%d).\n", strerror(errno), errno);
  modem_ctrl = (modem_ctrl_saved | TIOCM_RTS) & ~TIOCM_DTR;
  if (ioctl(port_fd, TIOCMSET, &modem_ctrl) == -1)
    printf("Error setting handshake lines: %s (%d).\n", strerror(errno), errno);
  sleep (delay);
  if (ioctl(port_fd, TIOCMSET, &modem_ctrl_saved) == -1)
    printf("Error setting handshake lines: %s (%d).\n", strerror(errno), errno);
  close(port_fd);
}

Hi there,
So does it get an IP address ? Is your DHCP working?
Do you have WPS turned on?
Lot’s to consider here. The reset button is required for initial boot of code after download to Xiao
after WiFi-Connect , disconnect and sleep can be used effectively.(sleep wakeup can be used to reset or resume.
HTH
GL :slight_smile: PJ

Curious to know if this code runs for you , The WPS example basically.
Press the WPS on your router. (either manually or from web page console)
Power on Xiao.

/*
THIS lightly tweeked PJG Example Code To Get ESP32c3 info from chip
 and to Connect WPS button AP and display RSSI, as well as do a BLE scan for devices.(WIP) concurrently 
 or as close as possible.
===========================================================
This example code provides both Push Button method and Pin
based WPS entry to get your ESP connected to your WiFi router.

Hardware Requirements
========================
ESP32 and a Router having WPS functionality

This code is under Public Domain License.

Author:
Pranav Cherukupalli <[email protected]>
*/

#include "WiFi.h"
#include "esp_wps.h"
/*
Change the definition of the WPS mode
from WPS_TYPE_PBC to WPS_TYPE_PIN in
the case that you are using pin type
WPS
*/
//#include "SimpleBLE.h"
#include <BLEDevice.h>
#include <BLEUtils.h>
#include <BLEScan.h>
#include <BLEAdvertisedDevice.h>
#include <U8x8lib.h>

#define ESP_WPS_MODE      WPS_TYPE_PBC
#define ESP_MANUFACTURER  "SEEED"
#define ESP_MODEL_NUMBER  "ESP32C3"
#define ESP_MODEL_NAME    "Xiao ESP"
#define ESP_DEVICE_NAME   "ESP STATION"


U8X8_SSD1306_128X64_NONAME_HW_I2C u8x8(/* reset=*/ U8X8_PIN_NONE);

uint32_t chipId = 0;
long SCB;
static esp_wps_config_t config;
void(* resetFunc) (void) = 0; //declare reset function @ address 0
int scanTime = 5; //In seconds
BLEScan* pBLEScan;

class MyAdvertisedDeviceCallbacks: public BLEAdvertisedDeviceCallbacks {
    void onResult(BLEAdvertisedDevice advertisedDevice) {
      //Serial.printf("Advertised Device: %s \n", advertisedDevice.toString().c_str());
    }
};

void setup(){
  Serial.begin(9600);
  delay(2000);
  u8x8.begin();
  u8x8.setFlipMode(1);   // set number from 1 to 3, the screen word will rotary 180*

  Serial.println();
   for(int i=0; i<17; i=i+8) {
	  chipId |= ((ESP.getEfuseMac() >> (40 - i)) & 0xff) << i;
	}

	Serial.printf("ESP32 Chip model = %s Rev %d\n", ESP.getChipModel(), ESP.getChipRevision());
	Serial.printf("This chip has %d cores\n", ESP.getChipCores());
  Serial.print("Chip ID: "); Serial.println(chipId);

  u8x8.setFont(u8x8_font_chroma48medium8_r);
  u8x8.setCursor(0, 0);
  u8x8.print("Looking for WPS");
	delay(2000);
  WiFi.onEvent(WiFiEvent);
  WiFi.mode(WIFI_MODE_STA);
  Serial.println("Starting WPS");
  wpsInitConfig();
  wpsStart();
  Serial.println("Scanning now...");
   while ( WiFi.status() != WL_CONNECTED) { //Wait for connection
   Serial.println(WiFi.localIP());
   delay(5000);
   // print the received signal strength:
  long rssi = WiFi.RSSI();
  Serial.print("RSSI:");
  Serial.println(rssi);
  Serial.println("Scanning...BLE too!");
  u8x8.setCursor(0, 3);
  u8x8.print("Scanning...BLE too!");
  BLEDevice::init("");
  pBLEScan = BLEDevice::getScan(); //create new scan
  pBLEScan->setAdvertisedDeviceCallbacks(new MyAdvertisedDeviceCallbacks());
  pBLEScan->setActiveScan(true); //active scan uses more power, but get results faster
  pBLEScan->setInterval(100);
  pBLEScan->setWindow(99);  // less or equal setInterval value
  //
  }
}
void loop(){
   //Serial.println(WiFi.localIP ());
 delay (2000);
 Serial.println("SoftwareReset");
  // put your main code here, to run repeatedly:
 // BLEScanResults foundDevices = pBLEScan->start(scanTime, false);
  //Serial.print("Devices found: ");
  //Serial.println(foundDevices.getCount());
  Serial.println("Scan done!");
  //pBLEScan->clearResults();   // delete results fromBLEScan buffer to release memory
  delay(10000);
 }


void wpsInitConfig(){
  config.wps_type = ESP_WPS_MODE;
  strcpy(config.factory_info.manufacturer, ESP_MANUFACTURER);
  strcpy(config.factory_info.model_number, ESP_MODEL_NUMBER);
  strcpy(config.factory_info.model_name, ESP_MODEL_NAME);
  strcpy(config.factory_info.device_name, ESP_DEVICE_NAME);
}

void wpsStart(){
    if(esp_wifi_wps_enable(&config)){
    	Serial.println("WPS Enable Failed");
    } else if(esp_wifi_wps_start(0)){
    	Serial.println("WPS Start Failed");
    }
}

void wpsStop(){
    if(esp_wifi_wps_disable()){
    	Serial.println("WPS Disable Failed");
    }
}
void resetfunc(){
  Serial.println("Soft reseting NOW");
  //NVIC_SystemReset();
}

String wpspin2string(uint8_t a[]){
  char wps_pin[9];
  for(int i=0;i<8;i++){
    wps_pin[i] = a[i];
  }
  wps_pin[8] = '\0';
  return (String)wps_pin;
}

void WiFiEvent(WiFiEvent_t event, arduino_event_info_t info){
  switch(event){
    case ARDUINO_EVENT_WIFI_STA_START:
      Serial.println("Station Mode");
      break;
    case ARDUINO_EVENT_WIFI_STA_GOT_IP:
      Serial.println("Connected to :" + String(WiFi.SSID()));
      Serial.print("Got IP: ");
      Serial.println(WiFi.localIP());
      delay (2000);
      //NVIC_SystemReset();      // processor software reset
      break;
    case ARDUINO_EVENT_WIFI_STA_DISCONNECTED:
      Serial.println("Disconnected , attempt reconnect ");
      WiFi.reconnect();
      break;
    case ARDUINO_EVENT_WPS_ER_SUCCESS:
      Serial.println("WPS Successfull, connecting to: " + String(WiFi.SSID()));
      wpsStop();
      delay(10);
      WiFi.begin();
      break;
    case ARDUINO_EVENT_WPS_ER_FAILED:
      Serial.println("WPS Failed, retrying");
      wpsStop();
      wpsStart();
      break;
    case ARDUINO_EVENT_WPS_ER_TIMEOUT:
      Serial.println("WPS Timedout, retrying");
      wpsStop();
      wpsStart();
      break;
    case ARDUINO_EVENT_WPS_ER_PIN:
      Serial.println("WPS_PIN = " + wpspin2string(info.wps_er_pin.pin_code));
      break;
    default:
      break;
  }
}

HTH :+1:

i do know i had a XIAO ESP32S3 that refused to connect to wifi… it would just go …
it was eventually determined it must have a defect… it also connected once or twice just long enough to drive crazy

Dear PJ,


Thank you for your response.

Both DCHP (home & work) are working fine. For WPS, I will try when back home (it’s 5:30 pm around here). Obviously I don’t have access to a WPS button at work.

For the IP, when I reboot the Xiao through the physical button, it get one from the Acess Point. But as I never connect otherwise, I don’t get an IP.

Since my last edit, I finally understood how to activate verbose logs. Here are the last version of my wifi code and the logs associated:

Type any key to continue: 
Initializing WiFi...
Putting module in STA mode ([  6210][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 0 - WIFI_READY
1)
Disconnecting from previous AP ([  6245][V][WiFiGeneric.cpp:340] _arduino_event_cb(): STA Started
[  6246][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 2 - STA_START
[  6267][V][WiFiGeneric.cpp:343] _arduino_event_cb(): STA Stopped
[  6268][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 3 - STA_STOP
1)
Connecting to WiFi... 
Putting module in STA mode ([  7280][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 0 - WIFI_READY
1)
Begining connection ([  7282][V][WiFiGeneric.cpp:340] _arduino_event_cb(): STA Started
[  7284][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 2 - STA_START
[  7344][V][WiFiGeneric.cpp:97] set_esp_interface_ip(): Configuring Station static IP: 0.0.0.0, MASK: 0.0.0.0, GW: 0.0.0.0
6)
Initial status: WL_DISCONNECTED
Waiting for connection: [  9153][V][WiFiGeneric.cpp:362] _arduino_event_cb(): STA Disconnected: SSID: SFR-5690, BSSID: 24:7f:20:9e:56:96, Reason: 2
[  9154][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 5 - STA_DISCONNECTED
[  9155][W][WiFiGeneric.cpp:1061] _eventCallback(): Reason: 2 - AUTH_EXPIRE
[  9155][D][WiFiGeneric.cpp:1081] _eventCallback(): WiFi Reconnect Running
[  9166][V][WiFiGeneric.cpp:97] set_esp_interface_ip(): Configuring Station static IP: 0.0.0.0, MASK: 0.0.0.0, GW: 0.0.0.0
[ 10263][V][WiFiGeneric.cpp:362] _arduino_event_cb(): STA Disconnected: SSID: SFR-5690, BSSID: 24:7f:20:9e:56:96, Reason: 2
[ 10264][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 5 - STA_DISCONNECTED
[ 10264][W][WiFiGeneric.cpp:1061] _eventCallback(): Reason: 2 - AUTH_EXPIRE
[ 10265][D][WiFiGeneric.cpp:1085] _eventCallback(): WiFi AutoReconnect Running
[ 10267][V][WiFiGeneric.cpp:97] set_esp_interface_ip(): Configuring Station static IP: 0.0.0.0, MASK: 0.0.0.0, GW: 0.0.0.0
[ 11287][V][WiFiGeneric.cpp:362] _arduino_event_cb(): STA Disconnected: SSID: SFR-5690, BSSID: 24:7f:20:9e:56:96, Reason: 2
[ 11288][D][WiFiGeneric.cpp:1039] _eventCallback(): Arduino Event: 5 - STA_DISCONNECTED
[ 11288][W][WiFiGeneric.cpp:1061] _eventCallback(): Reason: 2 - AUTH_EXPIRE
[ 11289][D][WiFiGeneric.cpp:1085] _eventCallback(): WiFi AutoReconnect Running
void init_wifi() {
  // Set WiFi to STA mode and disconnect from an AP if it was previously connected
  Serial.println("Initializing WiFi...");

  Serial.print("Putting module in STA mode (");
  Serial.print(WiFi.mode(WIFI_STA));
  Serial.println(")");

  Serial.print("Disconnecting from previous AP (");
  Serial.print(WiFi.disconnect(true, true));
  Serial.println(")");

  delay(1000);

  // Set WiFi to STA mode and connect to AP
  Serial.println("Connecting to WiFi... ");

  Serial.print("Putting module in STA mode (");
  Serial.print(WiFi.mode(WIFI_STA));
  Serial.println(")");

  Serial.print("Begining connection (");
  Serial.print(WiFi.begin(ssid, password));
  Serial.println(")");

  Serial.print("Initial status: ");
  print_wifi_status_label();
  Serial.println();

  delay(1000);

  Serial.print("Waiting for connection: ");
  WiFi.waitForConnectResult(WIFI_CONNECTION_TIMEOUT);
  print_wifi_status_label();
  Serial.println();
  
  // Retries if necessary
  while (WiFi.status() != WL_CONNECTED) {
    Serial.println("Retrying... ");

    Serial.print("Calling reconnect (");
    Serial.print(WiFi.reconnect());
    Serial.println(")");

    Serial.print("Waiting for connection: ");
    WiFi.waitForConnectResult(WIFI_CONNECTION_TIMEOUT);
    print_wifi_status_label();
    Serial.println();

    if (WiFi.status() == WL_CONNECT_FAILED) {
      delay(WIFI_CONNECTION_TIMEOUT);
    }
  }

  // Print IP address
  Serial.print("Obtained IP address: ");
  Serial.println(WiFi.localIP());
  Serial.println();
}

I seems to want to register an empty static IP. Next debug step on my side: try to force a static ip outside the DHCP range to see if it corrects the issue.

Hi there,
Here is some code I used a while back to help figure what I was doing.
It’s from Liam over at Arduino Forum.
It is a demo-code that has three useful additional functions,

// Demo-Code connect an ESP32 to a WiFi-network using stationmode STA

// stationmode is simply join the WiFi-network as your computer or smartphone does it
// the code has three useful functions one for easy identifiying the code in the flash
// one for non-blocking timing
// a heartbeat-blinker function for indicating the state the code is in

// the code is written with two programming rules:
// 1. put EACH functionality into its OWN function
// 2. give EACH function a SELF-explaining name what the function does
// you should follow these programming rules 
#include <WiFi.h>

const char *ssid     = "Your SSID";
const char *password = "your password";


void PrintFileNameDateTime() {
  Serial.println( F("Code running comes from file ") );
  Serial.println( F(__FILE__));
  Serial.print( F("  compiled ") );
  Serial.print(F(__DATE__));
  Serial.print( F(" ") );
  Serial.println(F(__TIME__));  
}


boolean TimePeriodIsOver (unsigned long &periodStartTime, unsigned long TimePeriod) {
  unsigned long currentMillis  = millis();  
  if ( currentMillis - periodStartTime >= TimePeriod )
  {
    periodStartTime = currentMillis; // set new expireTime
    return true;                // more time than TimePeriod) has elapsed since last time if-condition was true
  } 
  else return false;            // not expired
}

unsigned long MyTestTimer = 0;                   // variables MUST be of type unsigned long
const byte    OnBoard_LED = 2;


void BlinkHeartBeatLED(int IO_Pin, int BlinkPeriod) {
  static unsigned long MyBlinkTimer;
  pinMode(IO_Pin, OUTPUT);
  
  if ( TimePeriodIsOver(MyBlinkTimer,BlinkPeriod) ) {
    digitalWrite(IO_Pin,!digitalRead(IO_Pin) ); 
  }
}


void ConnectToWiFi() {
  WiFi.mode(WIFI_STA);
  Serial.println("WiFi.mode(WIFI_STA)");

  int myCount = 0;

  Serial.print("trying to connect to #");
  Serial.print(ssid);
  Serial.println("#");
  WiFi.begin(ssid, password);

  // Wait for connection
  while (WiFi.status() != WL_CONNECTED && myCount < 31) {
    BlinkHeartBeatLED(OnBoard_LED, 50); // blink LED fast during attempt to connect

    if ( TimePeriodIsOver(MyTestTimer, 500) ) { // once every 500 miliseconds
      Serial.print(".");                        // print a dot
       myCount++; 
       
      if (myCount > 30) { // after 30 dots = 15 seconds restart
        Serial.println();
        Serial.print("not yet connected executing ESP.restart();");
        ESP.restart();
      }
    }
  }

  if (WiFi.status() == WL_CONNECTED ) {
    Serial.println("");
    Serial.print("Connected to #");
    Serial.print(ssid);
    Serial.print("# IP address: ");
    Serial.println(WiFi.localIP());
  }

}

void setup() {
  Serial.begin(115200);
  Serial.println( F("Setup-Start") );
  PrintFileNameDateTime();
  ConnectToWiFi();
}

void PrintHelloMsg() {
  Serial.print( F("Hi there I'm the demo-code my IP address is: ") );
  Serial.println(WiFi.localIP());      
}


void loop() {
  BlinkHeartBeatLED(OnBoard_LED,500); // change blinking to a lower frequency indicating beeing connected

  if ( TimePeriodIsOver(MyTestTimer,1000) ) {
    PrintHelloMsg();
  }  
}



/*
most ESP32 boards have a blue LED connected to GPIO-pin 2
This blue LED is used to indicate state connecting to WiFi by blinking fast
state beeing connected to Wifi by blinking with 1 Hz

If the WiFi-connection is successfully established the serial monitor shows

08:44:02.915 -> Setup-Start
08:44:02.915 -> Code running comes from file 
08:44:02.915 -> your-path\ESP32-connect-to-Wifi-Demo-001\ESP32-connect-to-Wifi-Demo-001.ino
08:44:02.915 ->   compiled date/time of compiling
08:44:02.971 -> WiFi.mode(WIFI_STA)
08:44:02.971 -> trying to connect to #Your SSID#
08:44:03.362 -> ....
08:44:04.215 -> Connected to #Your SSID# IP address: given IP-adress NNN.NNN.NNN.NNN
08:44:04.865 -> Hi there I'm the demo-code my IP address is: NNN.NNN.NNN.NNN



if there is something wrong with your WiFi, SSID or password
you will see this in the serial monitor
08:32:36.598 -> Setup-Start
08:32:36.598 -> Code running comes from file 
08:32:36.598 -> F:\MyPortable-PRgs\arduino-1.8.16-newb\portable\sketchbook\ESP32-connect-to-Wifi-Demo-001\ESP32-connect-to-Wifi-Demo-001.ino
08:32:36.598 ->   compiled Dec  1 2021 08:32:18
08:32:36.684 -> WiFi.mode(WIFI_STA)
08:32:36.684 -> trying to connect to #your SSID#
08:32:37.036 -> ...............................
08:32:52.035 -> not yet connected executing ESP.restart();ets Jun  8 2016 00:22:57
08:32:52.035 -> 
08:32:52.035 -> rst:0xc (SW_CPU_RESET),boot:0x13 (SPI_FAST_FLASH_BOOT)
08:32:52.035 -> configsip: 0, SPIWP:0xee
08:32:52.035 -> clk_drv:0x00,q_drv:0x00,d_drv:0x00,cs0_drv:0x00,hd_drv:0x00,wp_drv:0x00
08:32:52.073 -> mode:DIO, clock div:1
08:32:52.073 -> load:0x3fff0018,len:4
08:32:52.073 -> load:0x3fff001c,len:1216
08:32:52.073 -> ho 0 tail 12 room 4
08:32:52.073 -> load:0x40078000,len:9720
08:32:52.073 -> ho 0 tail 12 room 4
08:32:52.073 -> load:0x40080400,len:6352
08:32:52.073 -> entry 0x400806b8
08:32:52.309 -> Setup-Start
08:32:52.309 -> Code running comes from file 
08:32:52.309 -> F:\MyPortable-PRgs\arduino-1.8.16-newb\portable\sketchbook\ESP32-connect-to-Wifi-Demo-001\ESP32-connect-to-Wifi-Demo-001.ino
08:32:52.309 ->   compiled Dec  1 2021 08:32:18
08:32:52.405 -> WiFi.mode(WIFI_STA)
08:32:52.405 -> trying to connect to #Your SSID#
08:32:52.758 -> ...............................
08:33:07.788 -> not yet connected executing ESP.restart();ets Jun  8 2016 00:22:57

 */

Be sure antenna is attached properly , what kind of RSSI 's are you seeing. Near and Far?
HTH
GL :slight_smile: PJ

Try this code if you have expansion board with SD installed

#include "FS.h"
#include "SD.h"
#include "SPI.h"
#include <time.h> 
#include <WiFi.h>

//#define SD_chipSelect D2 //XIAO 
#define SD_chipSelect 21 //XIAO ESP32S3 Cam Board

const char* ssid     = "your-ssid";
const char* password = "your-password";

long timezone = -5; 
byte daysavetime = 0;

void listDir(fs::FS &fs, const char * dirname, uint8_t levels)
{//Begin
  Serial.printf("Listing directory: %s\n", dirname);

  File root = fs.open(dirname);
  if(!root)
  {//Begin
    Serial.println("Failed to open directory");
    return;
  }//  End
  if(!root.isDirectory())
  {//Begin
    Serial.println("Not a directory");
    return;
  }//  End
  File file = root.openNextFile();
  while(file)
  {//Begin
    if(file.isDirectory())
    {//Begin
      Serial.print("  DIR : ");
      Serial.print (file.name());
      time_t t= file.getLastWrite();
      struct tm * tmstruct = localtime(&t);
      Serial.printf("  LAST WRITE: %d-%02d-%02d %02d:%02d:%02d\n",(tmstruct->tm_year)+1900,( tmstruct->tm_mon)+1, tmstruct->tm_mday,tmstruct->tm_hour , tmstruct->tm_min, tmstruct->tm_sec);
      if(levels)
      {listDir(fs, file.path(), levels -1);}
    }//  End 
    else 
    {//Begin
      Serial.print("  FILE: ");
      Serial.print(file.name());
      Serial.print("  SIZE: ");
      Serial.print(file.size());
      time_t t= file.getLastWrite();
      struct tm * tmstruct = localtime(&t);
      Serial.printf("  LAST WRITE: %d-%02d-%02d %02d:%02d:%02d\n",(tmstruct->tm_year)+1900,( tmstruct->tm_mon)+1, tmstruct->tm_mday,tmstruct->tm_hour , tmstruct->tm_min, tmstruct->tm_sec);
    }//  End
  file = root.openNextFile();
  }//  End
}//  End

void createDir(fs::FS &fs, const char * path)
{//Begin
  Serial.printf("Creating Dir: %s\n", path);
  if(fs.mkdir(path))
    {Serial.println("Dir created");} 
  else 
    {Serial.println("mkdir failed");}
}//  End

void removeDir(fs::FS &fs, const char * path)
{//Begin
  Serial.printf("Removing Dir: %s\n", path);
  if(fs.rmdir(path))
    {Serial.println("Dir removed");} 
  else 
    {Serial.println("rmdir failed");}
}//  End

void readFile(fs::FS &fs, const char * path)
{//Begin
  Serial.printf("Reading file: %s\n", path);
  File file = fs.open(path);
  if(!file)
  {//Begin
    Serial.println("Failed to open file for reading");
    return;
  }//  End
  Serial.print("Read from file: ");
  while(file.available())
  {Serial.write(file.read());}
  file.close();
}//  End

void writeFile(fs::FS &fs, const char * path, const char * message)
{//Begin
  Serial.printf("Writing file: %s\n", path);
  File file = fs.open(path, FILE_WRITE);
  if(!file)
  {//Begin
    Serial.println("Failed to open file for writing");
    return;
  }//  End
  if(file.print(message))
    {Serial.println("File written");}
  else 
    {Serial.println("Write failed");}
  file.close();
}//  End

void appendFile(fs::FS &fs, const char * path, const char * message)
{//Begin
  Serial.printf("Appending to file: %s\n", path);
  File file = fs.open(path, FILE_APPEND);
  if(!file)
  {//Begin
    Serial.println("Failed to open file for appending");
    return;
  }//  End
    if(file.print(message))
    {Serial.println("Message appended");}
  else 
    {Serial.println("Append failed");}
  file.close();
}//  End

void renameFile(fs::FS &fs, const char * path1, const char * path2)
{//Begin
  Serial.printf("Renaming file %s to %s\n", path1, path2);
  if (fs.rename(path1, path2)) 
    {Serial.println("File renamed");}
  else 
    {Serial.println("Rename failed");}
}//  End

void deleteFile(fs::FS &fs, const char * path)
{//Begin
  Serial.printf("Deleting file: %s\n", path);
  if(fs.remove(path))
    {Serial.println("File deleted");} 
  else 
    {Serial.println("Delete failed");}
}//  End

void setup()
{//Begin
  Serial.begin(19200);
  // We start by connecting to a WiFi network
  Serial.println();
  Serial.println();
  Serial.print("Connecting to ");
  Serial.println(ssid);
  WiFi.begin(ssid, password);
  while (WiFi.status() != WL_CONNECTED) 
  {//Begin
    delay(500);
    Serial.print(".");
  }//  End
  Serial.println("WiFi connected");
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());
  Serial.println("Contacting Time Server");
	configTime(3600*timezone, daysavetime*3600, "time.nist.gov", "0.pool.ntp.org", "1.pool.ntp.org");
	struct tm tmstruct ;
  delay(2000);
  tmstruct.tm_year = 0;
  getLocalTime(&tmstruct, 5000);
	Serial.printf("\nNow is : %d-%02d-%02d %02d:%02d:%02d\n",(tmstruct.tm_year)+1900,( tmstruct.tm_mon)+1, tmstruct.tm_mday,tmstruct.tm_hour , tmstruct.tm_min, tmstruct.tm_sec);
  Serial.println(""); 
  if(!SD.begin(SD_chipSelect))
  {//Begin
    Serial.println("Card Mount Failed");
    return;
  }//  End
  uint8_t cardType = SD.cardType();
  if(cardType == CARD_NONE)
  {//Begin
    Serial.println("No SD card attached");
    return;
  }//  End
  Serial.print("SD Card Type: ");
  if(cardType == CARD_MMC)
    {Serial.println("MMC");}
  else if(cardType == CARD_SD)
    {Serial.println("SDSC");} 
  else if(cardType == CARD_SDHC)
    {Serial.println("SDHC");} 
  else 
    {Serial.println("UNKNOWN");}
  uint64_t cardSize = SD.cardSize() / (1024 * 1024);
  Serial.printf("SD Card Size: %lluMB\n", cardSize);
  listDir(SD, "/", 0);
  removeDir(SD, "/mydir");
  createDir(SD, "/mydir");
  deleteFile(SD, "/hello.txt");
  writeFile(SD, "/hello.txt", "Hello ");
  appendFile(SD, "/hello.txt", "World!\n");
	listDir(SD, "/", 0);
  Serial.printf("All Done!....");
}//  End

void loop()
{}

Hi there,
You may want to “flush” serial port b4 the next connection, I have seen that jam up multiple wifi, ap connects…
HTH
GL :slight_smile: PJ

Hello all,


Thank you for all your responses. I progressed on the matter yesterday night at home. The board at home actually connects to the wifi but it takes an insane amount of time! I made multiple runs and it connects each time, after a delay between 4 and 12 minutes! So it appears using the hardware button was just shortening this waiting time to a reasonable amount.

The issue seems to be different at work, as I can not replicate the same behavior. While using the corporate wifi or my phone as Access Point. So my quest is not over :sweat_smile:.

In order to respond to all your suggestions:

  • @PJ_Glasso: Because I discovered that effect and was focuse don it, I didn’t try the WPS button yet
  • @PJ_Glasso: Yes, the antenne is attached properly. The board at home is about five meters from the Access Point with only a wood pannel between them (RSSI -63) and the board at work is maybe ten meters away in direct line of sight (RSSI -52 using my phone).
  • @cgwaltney: No SD attached but there is stuff in your code I wanted to use for debugging my issues (using a NTP server for logging in long runs for example). Thanks for it!
  • @PJ_Glasso: Flushing serial doesn’t seem to improve the issue for now


Martin.

Hello all,

Some updates on my tests of the wifi ability of the XIAO ESP32S3. I tried to switch from Arduino (and the library WiFi.h) to ESP-IDF (and the library esp_wifi.h). I don’t know the extend of their difference but I tried anyway.

On the Pi, the installation of ESP-IDF worked fine. But using the included “getting started” example failed as usual.

So my pain is not over…

Hi there,
So I’m feeling like there is something else at play Can post the compiler output first 3 lines and the last 20 line b4 the upload.? Can you post the exact code you are using? Even the code snips don’t compile with no includes?
You have a lot of variables in this particular setup. PLIO and Arduino are not the same so also pick one and get it working ,Then change or try the other environment. IMO your making it harder on yourself.

Are you on the windows or Linux and which IDE are you using, Normally if you run into an issue , I don’t see switching to a different IDE is going to help, as You can see it just complicates your scenario
and increases the frustration level.
Do you have more than one Xiao?
Have you visually inspected the build quality? Look around the antenna connection, (may need a magnifier) everything looks ok?
Are you using WPS2 security on the WiFi? (I use my phone as an access point to test occasionally and it works very well.) even Camera webserver example works with it. (sammy GS9+)
HTH
GL :slight_smile: PJ :v:

Look at this demo see if it opens some ideas.

Hello PJ,

I understand your point of view regarding adding complications while changing IDE. I suppose it’s just my experience in the academic world that makes me isolate each variable and test it independently…

Anyway, let me try to answer your questions/suggestions.

On the Xiao’s side, I have two of them. I checked the antennas under my company’s binocular microscope and they show no signs of bad mounting. This is also confirmed by the fact that scanning for wifi works on both item. I now have send the second item to one relative to see if the error stands between the chair and the screen… But the RSSI measured by the remaining item is equal to the RSSI measured by my phone when connected to the same AP.

On the Access Points’ sides, I tested four of them.

  • One at my work (for which I don’t have access to a WPS button for obvious security reasons)
  • One old linksys WRT54G at home (with WPS ; WPA2 authentication)
  • One of my internet provider’s hardware (with WPS ; WPA2 authentication)
  • My phone (without WPS ; WPA2 authentication)

On the computers I use to build and flash the programs, I use a windows 11 notebook (with both Arduino and VisualStudio+PlateformIO as IDE), and several raspberry pi 3 (with both Arduino and ESP-IDF as frameworks). As you say, I don’t think switching IDE is going to help. But at least I learned a lot by doing so (I also tried to flash the Xiao by piping the serial port from the RPi to a remote VM which was fun to do).

On the codes I use/used, they are the standard examples provided by SeeedStudio or Espressif:

As I understand it, all the chain of building, flashing and monitoring works (e.g. both SeeedStudio and Espressif wifi scans examples work fully with each Xiao and each computers).

To finish trying your suggestions, I finally tested today the WPS mode. On both my two personals AP. Again no success.

At work we used a different chip for a different project. And my teammate could connect to the wifi easily. I will try this chip to learn a bit more and drop the Xiao. Thank you very much for your time and your help. On my side I close the topic.

Hi there,
Well you certainly gave it the college try… :smiley: :+1:
FWIW, I found if I had the Arduino_BLE lib loaded in the arduino IDE. I had some code that would compile but not run, Until I removed it and recompiled… Long-Shot.

BOI, You made me miss for a millisecond :pinching_hand: the UNLIMITED :money_mouth_face:budget, that-my experience at the SEI in the burgh allowed, I could test until I was finished or at least said I was :laughing: :crossed_fingers:

GL :slight_smile: PJ

Dear All,

After a while, I decided to try the ESP32C3 instead of the ESP32S3 previously bought. So my company got two of them that I tried with the same programs/frameworks/wifi APs than before and… everything worked spot on! I don’t know exactly what is the issue with the S3 but at least I’m releived that it was not me!

There were some good ideas here, I think they helped my intermittent issues with wifi connection on esp32s3.

I’ve been working on the ESP32 device for over a year now. And I have also experienced intermittent connectivity and slow bandwidth issues. The RSSI strength is decent (around -40 to -50). But even with that, connectivity and or performance is sometime very poor. I switched to using Post antennas from Seeed and thought it helped. But a couple of days later, things just fell apart. But I did discover (quite by accident) that I get instant router connectivity and 3-4X increases in throughput with one simple move … holding the antenna. Works like a champ. That said, I really think the ESP32-S3 or the XIAO board needs some analysis. I will be trying other boards as well. But I don’t recall seeing this issue with the ESP32C3. Hmmmm. Sorry, I have no real solution. But I do see problems as well.

interesting!.. thanks for the information

Hey CG. I wanted to add a bit more info on the Wifi odyssey. I ordered and tested several different post-style antenna some of which boasted some impressive (but unlikely dB gains). The issue didn’t change. Wifi connectivity and performance was lethargic with these antenna. But grabbing the antenna seemed like the miracle fix. I also tried a stock Espressif dev board (ESP32S3 USB/OTG board). It just used a compact board/wafer antenna (soldered onto the PCB). And it seemed to work better. But when moved it to another room in the house, I got the same connectivity/performance issues. And once again, this was resolved by touching the antenna. So it’s not the XIAO board. I just purchase a TinySA Ultra Spectrum Analyzer to see if I can gain some insight into this sporadic issue. Till then, don’t try to adjust the horizontal or vertical (Twilight Zone)

some type of capacitive coupling… i also see this with my TV antenna… when i get close to move it the reception increases… when i move away to leave it alone… it gets worse

HI there,

So I would ask are the WAP /router you connect to on the same circuit or in different rooms?
Silly maybe have you checked the IG on the Plugs (the third prong) the computer is plugged into?
Are these on Battery or on USB-C ?

I’m suspicious of the WiFi on the S3 being handled by the 2 core, seems this wifi lib may not be up to it. The C3 works perfectly, The BSP’s may be why also. how many have been tested?
What happens if you attach a test clip from ant outside to ground?
I’m sure if you test and eliminate things it’s not you will figure it out…
HTH
GL :slight_smile: PJ :v:

Is there anybody who has anymore experience with this?
I really like the Seeed ESP32S3 Plus because of the extra memory etc.

However, I am also having problems with the connection, and not sure what the reason is.

I can’t find how to create a new post, so replied to this one. This is the debug output of the example on the Wiki combining the scan and connection example:

=========== Before Setup Start ===========
19:07:35.404 → Chip Info:
19:07:35.404 → ------------------------------------------
19:07:35.404 → Model : ESP32-S3
19:07:35.404 → Package : 0
19:07:35.404 → Revision : 0.02
19:07:35.404 → Cores : 2
19:07:35.404 → CPU Frequency : 240 MHz
19:07:35.404 → XTAL Frequency : 40 MHz
19:07:35.404 → Features Bitfield : 0x00000012
19:07:35.404 → Embedded Flash : No
19:07:35.404 → Embedded PSRAM : No
19:07:35.404 → 2.4GHz WiFi : Yes
19:07:35.404 → Classic BT : No
19:07:35.404 → BT Low Energy : Yes
19:07:35.404 → IEEE 802.15.4 : No
19:07:35.404 → ------------------------------------------
19:07:35.404 → INTERNAL Memory Info:
19:07:35.404 → ------------------------------------------
19:07:35.404 → Total Size : 364488 B ( 355.9 KB)
19:07:35.404 → Free Bytes : 326476 B ( 318.8 KB)
19:07:35.404 → Allocated Bytes : 32884 B ( 32.1 KB)
19:07:35.404 → Minimum Free Bytes: 322556 B ( 315.0 KB)
19:07:35.404 → Largest Free Block: 258036 B ( 252.0 KB)
19:07:35.404 → ------------------------------------------
19:07:35.404 → Flash Info:
19:07:35.404 → ------------------------------------------
19:07:35.404 → Chip Size : 16777216 B (16 MB)
19:07:35.404 → Block Size : 65536 B ( 64.0 KB)
19:07:35.404 → Sector Size : 4096 B ( 4.0 KB)
19:07:35.404 → Page Size : 256 B ( 0.2 KB)
19:07:35.404 → Bus Speed : 80 MHz
19:07:35.404 → Bus Mode : QIO
19:07:35.404 → ------------------------------------------
19:07:35.404 → Partitions Info:
19:07:35.404 → ------------------------------------------
19:07:35.404 → nvs : addr: 0x00009000, size: 20.0 KB, type: DATA, subtype: NVS
19:07:35.404 → otadata : addr: 0x0000E000, size: 8.0 KB, type: DATA, subtype: OTA
19:07:35.404 → app0 : addr: 0x00010000, size: 2048.0 KB, type: APP, subtype: OTA_0
19:07:35.404 → app1 : addr: 0x00210000, size: 2048.0 KB, type: APP, subtype: OTA_1
19:07:35.404 → ffat : addr: 0x00410000, size: 12160.0 KB, type: DATA, subtype: FAT
19:07:35.404 → coredump : addr: 0x00FF0000, size: 64.0 KB, type: DATA, subtype: COREDUMP
19:07:35.404 → ------------------------------------------
19:07:35.404 → Software Info:
19:07:35.404 → ------------------------------------------
19:07:35.404 → Compile Date/Time : Jul 12 2025 18:12:06
19:07:35.404 → Compile Host OS : macosx
19:07:35.404 → ESP-IDF Version : v5.4.2-25-g858a988d6e
19:07:35.404 → Arduino Version : 3.2.1
19:07:35.404 → ------------------------------------------
19:07:35.404 → Board Info:
19:07:35.404 → ------------------------------------------
19:07:35.404 → Arduino Board : XIAO_ESP32S3_PLUS
19:07:35.404 → Arduino Variant : XIAO_ESP32S3_Plus
19:07:35.404 → Arduino FQBN : esp32:esp32:XIAO_ESP32S3_Plus:UploadSpeed=921600,USBMode=hwcdc,CDCOnBoot=default,MSCOnBoot=default,DFUOnBoot=default,UploadMode=default,CPUFreq=240,FlashMode=qio,FlashSize=16M,PartitionScheme=fatflash,DebugLevel=verbose,PSRAM=disabled,LoopCore=1,EventsCore=1,EraseFlash=none,JTAGAdapter=default
19:07:35.404 → ============ Before Setup End ============
19:07:35.501 → [ 519][I][esp32-hal-periman.c:141] perimanSetPinBus(): Pin 19 already has type USB_DM (45) with bus 0x3fc9a9f4
19:07:35.501 → [ 519][I][esp32-hal-periman.c:141] perimanSetPinBus(): Pin 20
19:07:35.535 → [ 531][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 101 - WIFI_READY
19:07:35.567 → [ 575][W][STA.cpp:543] disconnect(): STA already disconnected.
19:07:35.567 → [ 576][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 110 - STA_START
19:07:35.567 → [ 577][V][STA.cpp:110] _onStaArduinoEvent(): Arduino STA Event: 110 - STA_START
19:07:35.667 → scan start
19:07:38.465 → us: 0, Results: 18
19:07:38.465 → [ 3465][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 102 - SCAN_DONE
19:07:38.465 → scan done
19:07:38.465 → 18 networks found
19:07:38.465 → 1: AAAA (-62)*
19:07:38.465 → 2: BBBB (-62)*
19:07:38.497 → 3: CCCC (-62)
19:07:38.497 → 4: CCCC (-64)
19:07:38.497 → 5: BBBB (-65)*
19:07:38.497 → 6: AAAA (-65)*
19:07:38.529 → 7: CCCC (-90)
19:07:38.529 → 8: AAAA (-90)*
19:07:38.529 → 9: BBBB (-92)*
19:07:38.561 → 10: BBBB (-93)*
19:07:38.628 →
19:07:38.661 → Connecting to WiFi …AAAA, BSSID: 36:87:ba:e5:d0:3c, Reason: 2
19:07:39.681 → [ 4674][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 113 - STA_DISCONNECTED
19:07:47.933 → MS, BSSID: 36:87:ba:e5:cd:3e, Reason: 2
19:07:47.933 → [ 12941][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 113 - STA_DISCONNECTED
19:07:47.933 → [ 12942][V][STA.cpp:110] _onStaArduinoEvent(): Arduino STA Event: 113 - STA_DISCONNECTED
19:07:47.933 → [ 12942][W][STA.cpp:137] _onStaArduinoEvent(): Reason: 2 - AUTH_EXPIRE
19:07:47.933 → [ 12942][D][STA.cpp:158] _onStaArduinoEvent(): WiFi AutoReconnect Running
19:07:47.933 → [ 12943][W][STA.cpp:543] disconnect(): STA already disconnected.

It then keeps repeating the lines:

19:07:40.630 → .MS, BSSID: 36:87:ba:e5:d0:3c, Reason: 2
19:07:40.697 → [ 5700][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 113 - STA_DISCONNECTED
19:07:40.697 → [ 5701][V][STA.cpp:110] _onStaArduinoEvent(): Arduino STA Event: 113 - STA_DISCONNECTED
19:07:40.697 → [ 5701][W][STA.cpp:137] _onStaArduinoEvent(): Reason: 2 - AUTH_EXPIRE
19:07:40.697 → [ 5702][D][STA.cpp:158] _onStaArduinoEvent(): WiFi AutoReconnect Running
19:07:40.697 → [ 5702][W][STA.cpp:543] disconnect(): STA already disconnected.
19:07:41.714 → [ 6724][V][NetworkEvents.cpp:117] _checkForEvent(): Network Event: 113 - STA_DISCONNECTED
19:07:41.714 → [ 6725][V][STA.cpp:110] _onStaArduinoEvent(): Arduino STA Event: 113 - STA_DISCONNECTED
19:07:41.714 → [ 6725][W][STA.cpp:137] _onStaArduinoEvent(): Reason: 2 - AUTH_EXPIRE
19:07:41.714 → [ 6726][D][STA.cpp:158] _onStaArduinoEvent(): WiFi AutoReconnect Running
19:07:41.714 → [ 6726][W][STA.cpp:543] disconnect(): STA already disconnected.

One thing I noticed on an earlier run with more verbose messaging is three notices I cannot place:

  • st. external pin
  • rst external pin
  • external pin.

It seems to me on the rare occasion the device connects it is always with a rat external pin just before it, but I can find no information on what it means.