Issue with Bus Servo Driver Board and Pico 2 over UART

Dear community,

I am having trouble trying to control a Feetech STS3215 through a Bus Servo Driver Board with a Raspberry Pi Pico 2 over UART.

The Driver Board works fine over USB, I can move the motor with a workstation and the scservo_sdk library.

When moving onto the Pico 2, I’ve been trying to simply ping the motor as especified in the Feetech protocol. I know with certainty its ID and baudrate, as I can previously set those via USB. As stated in the documentation, I have removed the jumper cap and connected the Pico TX with the Driver Board RX, and vice versa. Note that the pads JP1 and JP2 are soldered in my v1.0 board, though it should have nothing to do with UART.

All I seem to get is an echo of my ping, and even other random messages. I have confirmed this both by adapting the scservo example, and by creating my own MicroPython script. Even if no motor is connected to the Driver Board I get a reply, which makes no sense. I have checked with a multimiter, but the RX and TX pins of the board are not shorted. I have reproduced this issue with two different Driver Boards, Feetech motors and Pico 2 boards.

I would appreciate any help.

Hi there,

So, I have a couple on the bench , getting ready for some project setup and test.
I don’t think it’s a Pico logic-level or polarity problem.
That “I get a reply even with no servo connected” is the giveaway: you’re not actually talking to the servo bus — you’re seeing the board itself / the USB-UART path echoing or driving the line.

What’s most likely happening

On the Bus Servo Driver Board, there are two different modes, and they’re selected by hardware jumpers/solder bridges:

  • UART (MCU) mode: use the RX/TX pins to a microcontroller, and do not short the 2-pin header. :backhand_index_pointing_left: :saluting_face: WRONG, I had to Short it to work
  • USB mode: you must bridge the solder pads on the back and short the front 2-pin header.

You say: JP1/JP2 are soldered on v1.0. That sounds exactly like the board is still configured as “USB path active,” so the USB-UART circuitry can end up loading/driving the UART pins. That can produce:

  • echo of your own ping
  • garbage/random bytes
  • “responses” even when no servo is attached

Try this

  1. Put the board into true UART mode
  • Remove the solder bridge on the back pads (JP1/JP2) so those pads are open (UART mode). (USB mode requires them bridged .)
  • Make sure the front 2-pin is NOT shorted (UART mode expects it open ).
  • Unplug USB from the driver board while testing UART-to-Pico (so the USB-UART chip isn’t powered and fighting the line).
  1. Verify with a dead-simple electrical test
  • With no servo connected, send bytes from Pico.
  • If the board “replies” again, it’s still not in UART mode or the board TX is being driven by something else.
  1. Then worry about the usual UART basics
  • Pico UART should be 8N1 at the known baud, common ground, correct TX↔RX crossing.
  • Servo power must be correct (STS series often wants higher than 5V).

Because in USB mode the board is intentionally configured as a USB-UART bridge; in your case, that same bridge is likely still “in circuit” when you try to use the external RX/TX pins — so they aren’t getting a clean path to the servo bus.

If you want, paste me the exact photo/labeling of your v1.0 board back side (JP pads) and I’ll tell you exactly which bridge to open and what “UART mode” should look like.

HTH
GL :slight_smile: PJ :v:

Thanks for the reply. I will not be able to remove the solder bridge on the back pads until early next week. I’ll let you know then!

So, I have a couple on the bench , getting ready for some project setup and test.

If you are able to use UART, I would appreciate if you let me know.

Best,

Martinho

Hey @PJ_Glasso,

I have unsuccessfully tried the following:

  1. Remove the solder bridge on back pads (checked that with a multimiter)
  2. Make sure the front 2 pin is NOT shorted
  3. Unplug USB

:x: I still see the echo.

So, I have a couple on the bench , getting ready for some project setup and test.

Where you able to communicate via UART on your own setup? Maybe you can share the details of your hardware connection and the scripts you have used, if so.

Best,

Martiño

Hi there,

So , Sorry for the late reply.
Had a Loss in the Family so was away from the LAb :wink:
I still have it here and on Deck, time permitting I will set it up this evening with some solid results and demo, with code and video to follow.

HTH
GL :slight_smile: PJ :v:

looks like you gave it the college try, I 'll see what I can find. :+1:

Hi there,

So I was able to perform all the tests and Work with both modes and two servos.
Bottom line Everything works! :+1:

USB mode = Jumper on Top & Solder Bridges on Bottom.

Commands to move or init servos come from a USB host (terminal) by way of a Python script or dedicated control program.
Find your com port… First step.

I used a Python Script to change the ID of one of the Servos. (always power off after)
I used another to verify the ID’s
I used a third to Send position commands to each.
I used a forth “follower.py” to have one as a Master and the other as a Slave.
WORKS PERFECTLY!

Now UART Mode… :sweat_smile: :crossed_fingers:
A Xiao C3 is now able to send the commands directly to the servo and the USB on the Xiao can be used to send command through the Xiao serial port to the servos as well.
This code allows just that,
Enter the command on the Serial port terminal in Arduino and move the servos directly. Truly interactive , :grin:
Your code can move and respond to Sensor data and move the Servos, if you want to make a fine adjustment, enter it in the terminal. Or Leave it Out!

I used the SCServo Lib as instructed by the Wiki.

UART MODE - NO Solder Bridges in Place and the Jumper IS Installed on the TOP

Xiao C3 is in the slot… executing the attached Sketch, This is the Serial output

========================================
XIAO ESP32C3 UART Dual Servo Control
Rev 1.1  |  2026-03-19
Library: SCServo
Boot button self-test enabled
========================================
Pinging servos...
Servo 1: DETECTED
Servo 2: DETECTED

Reading initial positions...
Servo 1 position: 2047
Servo 2 position: 2047

Centering both servos...
Moved both -> S1: 2048  S2: 2048
Running startup demo...
Moved both -> S1: 2048  S2: 2048
Moved both -> S1: 1000  S2: 3000
Moved both -> S1: 3000  S2: 1000
Moved both -> S1: 2048  S2: 2048
Startup demo done.
========== Servo Command Help ==========
c        -> center both servos
l        -> servo1 left, servo2 right
r        -> servo1 right, servo2 left
m        -> run startup demo
t        -> run boot-button self-test demo
1 xxxx   -> move servo 1 to position xxxx
2 xxxx   -> move servo 2 to position xxxx
b xxxx   -> move both servos to position xxxx
h        -> show this help
Position range: 0 to 4095
========================================

Press the BOOT button anytime to run the self-test demo.

Moved both -> S1: 2048  S2: 2048
Moved both -> S1: 2048  S2: 2048
Running startup demo...
Moved both -> S1: 2048  S2: 2048
Moved both -> S1: 1000  S2: 3000
Moved both -> S1: 3000  S2: 1000
Moved both -> S1: 2048  S2: 2048
Startup demo done.
Boot button pressed -> running self-test demo

========================================
BOOT BUTTON SELF-TEST START
========================================
Moved both -> S1: 2048  S2: 2048
Step 1: 90 degrees one way
Moved both -> S1: 3072  S2: 3072
Step 2: 180 degrees the other way
Moved both -> S1: 1024  S2: 1024
Step 3: reverse back
Moved both -> S1: 2560  S2: 2560
Step 4: wide sweep
Moved both -> S1: 0  S2: 0
Moved both -> S1: 4095  S2: 4095
Step 5: pause
Moved both -> S1: 2048  S2: 2048
Step 6: goodbye wave
Goodbye wave...

You can see it at the end of the Video. :grin: :waving_hand:

Here is the code…

  /*
  ============================================================
  Project : XIAO ESP32C3 + Seeed Servo Driver Board UART Test
  Board   : Seeed Studio XIAO ESP32C3
  Servos  : STS-3215 (IDs 1 and 2)
  Library : SCServo
  Rev     : 1.1
  Date    : 2026-03-19
  Author  : PJ Glasso & EAILLM
  Features:
  - UART mode servo control
  - Ping servo IDs 1 and 2
  - Startup motion demo
  - Serial Monitor command control
  - Boot button self-test / wow demo

  Hardware notes:
  - Board in UART mode
  - Top jumper installed
  - Bottom solder bridges NOT installed
  - External 12V servo power connected
  - Servo IDs must already be unique (1 and 2)

  Serial Monitor commands:
  c        -> center both servos
  l        -> servo1 left, servo2 right
  r        -> servo1 right, servo2 left
  m        -> middle demo move
  t        -> run boot-button self-test demo
  1 2048   -> move servo 1 to position 2048
  2 1024   -> move servo 2 to position 1024
  b 1500   -> move both servos to position 1500
  h        -> show help
  ============================================================
*/

#include <SCServo.h>

SMS_STS st;

#define SERVO_SERIAL Serial0

// XIAO ESP32C3 Boot button is commonly on GPIO 9
#define BOOT_BUTTON_PIN 9

// ---------------- Servo configuration ----------------
const uint8_t SERVO1_ID = 1;
const uint8_t SERVO2_ID = 2;

const int SERVO_MIN_POS = 0;
const int SERVO_MAX_POS = 4095;
const int SERVO_CENTER  = 2048;

// Motion tuning
const uint16_t MOVE_SPEED = 1500;
const uint8_t  MOVE_ACC   = 50;

// Button handling
bool lastButtonState = HIGH;
unsigned long lastDebounceTime = 0;
const unsigned long debounceDelay = 40;

// -----------------------------------------------------

int clampPosition(int pos) {
  if (pos < SERVO_MIN_POS) return SERVO_MIN_POS;
  if (pos > SERVO_MAX_POS) return SERVO_MAX_POS;
  return pos;
}

void printHelp() {
  Serial.println();
  Serial.println("========== Servo Command Help ==========");
  Serial.println("c        -> center both servos");
  Serial.println("l        -> servo1 left, servo2 right");
  Serial.println("r        -> servo1 right, servo2 left");
  Serial.println("m        -> run startup demo");
  Serial.println("t        -> run boot-button self-test demo");
  Serial.println("1 xxxx   -> move servo 1 to position xxxx");
  Serial.println("2 xxxx   -> move servo 2 to position xxxx");
  Serial.println("b xxxx   -> move both servos to position xxxx");
  Serial.println("h        -> show this help");
  Serial.println("Position range: 0 to 4095");
  Serial.println("========================================");
  Serial.println();
}

void moveServo(uint8_t id, int pos, uint16_t speed = MOVE_SPEED, uint8_t acc = MOVE_ACC) {
  pos = clampPosition(pos);
  st.WritePosEx(id, pos, speed, acc);

  Serial.print("Moved servo ");
  Serial.print(id);
  Serial.print(" to ");
  Serial.println(pos);
}

void moveBoth(int pos1, int pos2, uint16_t speed = MOVE_SPEED, uint8_t acc = MOVE_ACC) {
  uint8_t ids[2] = {SERVO1_ID, SERVO2_ID};
  s16 positions[2] = {(s16)clampPosition(pos1), (s16)clampPosition(pos2)};
  u16 speeds[2] = {speed, speed};
  byte accs[2] = {acc, acc};

  st.SyncWritePosEx(ids, 2, positions, speeds, accs);

  Serial.print("Moved both -> S1: ");
  Serial.print(positions[0]);
  Serial.print("  S2: ");
  Serial.println(positions[1]);
}

void centerBoth() {
  moveBoth(SERVO_CENTER, SERVO_CENTER);
}

void pingServo(uint8_t id) {
  int result = st.Ping(id);

  Serial.print("Servo ");
  Serial.print(id);
  Serial.print(": ");

  if (result != -1) {
    Serial.println("DETECTED");
  } else {
    Serial.println("NOT DETECTED");
  }
}

void readPositions() {
  int pos1 = st.ReadPos(SERVO1_ID);
  int pos2 = st.ReadPos(SERVO2_ID);

  Serial.print("Servo 1 position: ");
  Serial.println(pos1);

  Serial.print("Servo 2 position: ");
  Serial.println(pos2);
}

void startupDemo() {
  Serial.println("Running startup demo...");

  centerBoth();
  delay(1200);

  moveBoth(1000, 3000);
  delay(1200);

  moveBoth(3000, 1000);
  delay(1200);

  centerBoth();
  delay(1200);

  Serial.println("Startup demo done.");
}

void goodbyeWave() {
  Serial.println("Goodbye wave...");

  int base = SERVO_CENTER;
  int wave = 220;

  for (int i = 0; i < 3; i++) {
    moveBoth(base - wave, base - wave, 1200, 40);
    delay(350);
    moveBoth(base + wave, base + wave, 1200, 40);
    delay(350);
  }

  centerBoth();
  delay(500);
}

void selfTestDemo() {
  Serial.println();
  Serial.println("========================================");
  Serial.println("BOOT BUTTON SELF-TEST START");
  Serial.println("========================================");

  // Start from center
  centerBoth();
  delay(1000);

  // About 90 degrees one way
  Serial.println("Step 1: 90 degrees one way");
  moveBoth(3072, 3072, 1400, 50);
  delay(1400);

  // About 180 degrees the other way
  Serial.println("Step 2: 180 degrees the other way");
  moveBoth(1024, 1024, 1500, 50);
  delay(1600);

  // Reverse back toward center/right
  Serial.println("Step 3: reverse back");
  moveBoth(2560, 2560, 1400, 50);
  delay(1300);

  // Wider 360-ish style sweep across a large range
  Serial.println("Step 4: wide sweep");
  moveBoth(0, 0, 1700, 60);
  delay(1800);

  moveBoth(4095, 4095, 1700, 60);
  delay(2200);

  // Pause
  Serial.println("Step 5: pause");
  centerBoth();
  delay(1200);

  // Small goodbye wave
  Serial.println("Step 6: goodbye wave");
  goodbyeWave();

  Serial.println("SELF-TEST COMPLETE");
  Serial.println("========================================");
  Serial.println();
}

void processSerialCommand() {
  if (!Serial.available()) return;

  String line = Serial.readStringUntil('\n');
  line.trim();

  if (line.length() == 0) return;

  if (line.equalsIgnoreCase("h")) {
    printHelp();
    return;
  }

  if (line.equalsIgnoreCase("c")) {
    centerBoth();
    return;
  }

  if (line.equalsIgnoreCase("l")) {
    moveBoth(1000, 3000);
    return;
  }

  if (line.equalsIgnoreCase("r")) {
    moveBoth(3000, 1000);
    return;
  }

  if (line.equalsIgnoreCase("m")) {
    startupDemo();
    return;
  }

  if (line.equalsIgnoreCase("t")) {
    selfTestDemo();
    return;
  }

  char cmd = line.charAt(0);
  int spaceIndex = line.indexOf(' ');

  if (spaceIndex < 0) {
    Serial.println("Invalid command. Type 'h' for help.");
    return;
  }

  String valueStr = line.substring(spaceIndex + 1);
  valueStr.trim();

  int pos = clampPosition(valueStr.toInt());

  switch (cmd) {
    case '1':
      moveServo(SERVO1_ID, pos);
      break;

    case '2':
      moveServo(SERVO2_ID, pos);
      break;

    case 'b':
    case 'B':
      moveBoth(pos, pos);
      break;

    default:
      Serial.println("Unknown command. Type 'h' for help.");
      break;
  }
}

void checkBootButton() {
  bool reading = digitalRead(BOOT_BUTTON_PIN);

  if (reading != lastButtonState) {
    lastDebounceTime = millis();
  }

  if ((millis() - lastDebounceTime) > debounceDelay) {
    static bool buttonHandled = false;

    // Active low button press
    if (reading == LOW && !buttonHandled) {
      Serial.println("Boot button pressed -> running self-test demo");
      selfTestDemo();
      buttonHandled = true;
    }

    if (reading == HIGH) {
      buttonHandled = false;
    }
  }

  lastButtonState = reading;
}

void setup() {
  pinMode(BOOT_BUTTON_PIN, INPUT_PULLUP);

  Serial.begin(115200);
  delay(2000);

  Serial.println();
  Serial.println("========================================");
  Serial.println("XIAO ESP32C3 UART Dual Servo Control");
  Serial.println("Rev 1.1  |  2026-03-19");
  Serial.println("Library: SCServo");
  Serial.println("Boot button self-test enabled");
  Serial.println("========================================");

  SERVO_SERIAL.begin(1000000);
  st.pSerial = &SERVO_SERIAL;

  delay(200);

  Serial.println("Pinging servos...");
  pingServo(SERVO1_ID);
  pingServo(SERVO2_ID);

  Serial.println();
  Serial.println("Reading initial positions...");
  readPositions();

  Serial.println();
  Serial.println("Centering both servos...");
  centerBoth();
  delay(1200);

  startupDemo();
  printHelp();
  Serial.println("Press the BOOT button anytime to run the self-test demo.");
}

void loop() {
  processSerialCommand();
  checkBootButton();
}

Remove the USB cable , and Press the boot button for a selftest hands-Free.
GL
HTH
AMA
PJ
:v:

Hi there,

So, in Summary…

I used a Basic [email protected] A, meanwell Power supply for the test connected to the Servo Driver Board, both modes are tested. USB / Bridge & UART / Local. Be sure they match, don’t get cute with the connections. :face_with_hand_over_mouth:
Servos are 12Vdc (STS3215 FeeTech) and daisy chained ID one(1) is first and ID (2) is second.
This is the holder for the tests…
https://makerworld.com/en/models/1861690-servo-motor-clamp-for-sts3215-bench-test-mount?from=search#profileId-1991270

Pics of the board, shows one with bridges, (USB) and one without Bridges (UART)
“Can anyone find the Bridge”
Extra Points if you know which song that is from :grin: LOL

In both cases the JUMPER(yellow) is INSTALLED on the top of the Board.


Bridged…

No bridge…

Why do they shoot themselves in the Foot? If the Jumper is used or required in both USE cases, why ship it without one, AGAIN with the BAD out of the BOX/BAG experience. Penny Wise and Pound Foolish… :face_with_hand_over_mouth:in order to save a penny and the cost to put it on before shipping?

A solder Bridge ? REALLY…no that is equally NON starter type crap there.
A user must solder on it before they even know if it works… BLAHHHH :sweat_smile:

What is needed…

A) there are errors in the WiKI . fix those.
B) Someone should sit down with two servos, one or Two Driver bords and walk thru the WiKI, You will see what is Missing and incorrect pretty fast.
Because if you follow it , Nothing really works. The Jumper info Especially is incorrect and confusing ALL at the same time.
(needs WORK)
C) (in my best ESPN Voice) :face_with_open_eyes_and_hand_over_mouth: C’mon MAN!.. You guys need to put a few more minutes in the enclosure for it… :squinting_face_with_tongue: You see what I did, You don’t want a LIVE- 12vdc board flopping around like an NBA player. I afixed the one I got and printed (yello) from Thingiverse to the Servo test holder(Seeed Grreeen) :star_struck:. As you can see it doesn’t fit the top if you put a XIAO on the board.

The Board works very, very well. once you get it figured out.

HTH
GL :slight_smile: PJ :v:

I used a separate 3v3 power supply (eg from Pico 2) for the non USB mode, plugged in to the XIAO 3v3 pin (12).
Jumper off.
Pads desoldered.

Example.

Hi there,

OK, so here is the Servo board case from lebotheads.
servo_driver_case_lid.step.zip (185.3 KB)

I resliced to leave off the dinRail tab :v:

GL :slight_smile: PJ :v: