I recently purchased the Jetson AGX Xavier H01 Kit from Seeed: https://www.seeedstudio.com/Jetson-Xavier-AGX-H01-Kit-p-5283.html?queryID=de0a9bd5236e5e86e4ed85c3b8fd3f08&objectID=5283&indexName=bazaar_retailer_products
While attempting to flash it multiple times, I received the following error code from the Nvidia SDKManager:
The target is in a bad state
The Jetson target is in a bad state and cannot be flashed. Please manually put the target into recovery mode and then try flashing
I am flashing from a host OS with Ubuntu 20.04 using the USB-C port located on the front of the board. I am attempting to flash Jetpack version 5.0.2 and I have attempted flashing over 5 times. Usually, reopening Jetpack, power cycling the Jetson, or disconnecting and reconnecting the USB does the trick, but this was not the case this time.
I have flashed multiple Jetson AGX Xavier’s from the official Nvidia site. Has anyone seen this issue and has still had success flashing their board(s)?