Is the WS2813B compatible with the raspberry pi

Is the WS2813B compatible with the raspberry pi? I do not mind stepping the voltage like the Adafruit WS2812. If so does it need different libraries than the WS2812?

Hello,

the code of WS2812B also works well with

WS2813B, pls refer to https://tutorials-raspberrypi.com/connect-control-raspberry-pi-ws2812-rgb-led-strips/

Thanks

best rgds
Mancy