so I had my bluetooth bee connected to a PC for a short time, long enough to set it to slave mode. Now whenever I contact it I get nothing but “ERROR”
For instance this is what I see after resetting it and trying to set the mode again using sscom3.2 and windos 7 64bit:
[code]WORK:SLAVER
+BTSTATE:0
+BTSTATE:1
ERROR
[/code]
the command I am sending is +STWMOD=1 and everything else should still be default 38400, I have the check box for send new checked.
I have also read through viewtopic.php?f=4&t=687 and it provides no helpful information.
computer -> USB cable -> UartSBee -> Bluetooth bee
It also doesnt matter what command I send it they all give error. I have tried multiple commands from: seeedstudio.com/wiki/Bluetooth_Bee