What’s the brightness spec for the 11.6inch HDMI LCD (H) (with case), 1920*1080, IPS, Capacitive touch, Support Raspberry Pi 4 SKU 104990623
Hi ,
what kind of parameters are you looking for brightness spec?
This is the WiKi page: <LINK_TEXT text=“https://www.waveshare.com/wiki/11.6inch … with_case)”>https://www.waveshare.com/wiki/11.6inch_HDMI_LCD_(H)_(with_case)</LINK_TEXT>
IPS (in-plane switching) is a screen technology for liquid-crystal displays (LCDs). It was … Further improvement in viewing angle; 10 percent increase in brightness; Up to 15 percent decrease in production costs; Increased image quality.
i recently bought an ips display that is 250 in brightness but it is much brighter than my old va display that is also 250, how bright must a va or tn display be to equal the 250 ips? what about led tvs brightness and picture quality compared to how nice the picture looks for the 250 ips display? pls help ty and i was looking at the alienware, pcs, it offered to hardware one that is nvme but there is " (boot)" next to it, what does this mean? can i use it as a normal hard drive,