Hi,
I’m following ST wiki regarding STM32MP157C-DK2, using it I’ve build linux-stm32mp-5.4.31.r0 but there isn’t the dts for ODYSSEY STM32MP157C available in it.
I’ve seen that for ODYSSEY STM32MP157C it is available only Linux 4.19.9
and u-boot:
and these overlays:
but these overlays can be used for linux-stm32mp-5.4.31.r0?
I’ve to use sudo make install_rpi in this case?
Thanks,
Antonio