Does the Odyssey support hardware time-stamping support for ieee 1588/PTPv2 with Linux and PTP4l? I see the Intel ethernet chip does support it. Has the appropriate software driver et al been incorporated and tested for timestamped PTPv2 use? If so, does that include success if run the following command under Linux, ethtool -T eth0, that will receive indication of hardware timestamping?