How to program WIO-5E mini (Seeed) using ST-LINK/V2 mini

Hello everyone , i 've got a problem to connect my stlink with stm32cube programmer after a week of research i can’t connect it back. When i’ve tryed the first time i could make it , even before with at command i could connect my stm32wlE5JC wio 5 mini to my gateway server.

here my logs:

---- Opened the serial port /dev/tty.usbserial-1120 ----
15:88:09:CF:4F:3C

DevEui: 00:80:E1:15:05:99:98:B8

####Hz at DR 0
1s524:MAC txDone
6s558:RX_1 on freq 868100000 Hz at DR 0
6s755:IRQ_RX_TX_TIMEOUT
6s756:MAC rxTimeOut
7s558:RX_2 on freq 869525000 Hz at DR 0
7s755:IRQ_RX_TX_TIMEOUT
7s756:MAC rxTimeOut

= JOIN FAILED

30s041:temp= 26
30s041:VDDA= 254
30s045:TX on freq 868300000 Hz at DR 0
31s532:MAC txDone
36s566:RX_1 on freq 868300000 Hz at DR 0
36s763:IRQ_RX_TX_TIMEOUT
36s764:MAC rxTimeOut
37s566:RX_2 on freq 869525000 Hz at DR 0
37s763:IRQ_RX_TX_TIMEOUT
37s764:MAC rxTimeOut

= JOIN FAILED

How can i reboot to the builtin state.

Impossible for me to connect back with my stlink v2.
Iv’e readen loads of thinks , tryed many thinks but i can’t fidn out.

NB. I’m still got one new stm32wl which i didn’t touch yet…

Can someone help me to find out my problem many thanks in advance.

Interesting Question