How to program a LoRa-E5

Do you know if the SWO pin from the STM32WL is exposed? So far, I’ve only been able to program the module using the directions on the wiki using SWDIO and SWCLK. For printf debugging, I’ve had to just use the UART to USB bridge. That said, I would like to be able to use the serial wire viewer instead if possible. Without the schematic for the module internals, I’ve been left to guess. Thanks!