How to install jetpack 5.0.2 into Jetson Xavier NX

I sussesufully install jetpack5.0.2, and here is what I do.

Step1.Install jetson os into nvme

Step2. Install jetson os into emmc

Step3. set boot order make ssd first

Step4. install sdk component to nvme

I assum there have two way we can expand the disk(correct me if I’m wrong)

  1. Native boot from SSD(kernal and roofs are in the SSD instead of emmc)

  2. This mounts the root filesystem to external memory, but we still need to use the emmc in order to boot the device