I’m using ODYSSEY STM32MP157C development Kit, it has only two boot modes (eMMC and SDCard), I want to use USB Boot mode for fimrware flashing.
How to setup the USB boot mode for flashing firmware ?
I’m using ODYSSEY STM32MP157C development Kit, it has only two boot modes (eMMC and SDCard), I want to use USB Boot mode for fimrware flashing.
How to setup the USB boot mode for flashing firmware ?
Sorry, the hardware doesnt support USB boot mode.
We’re designing custom baseboard using ODYSSEY STM32MP157C SoM, I referred the STM32MP157C-DK2 dev kit from STM, they’re using USB_DP2 and USB_DM2 in USB Type C connector.
Here is the USB Type C schematics of STM32MP157C-DK2,
Can i follow the STM32MP157C-DK2 circuit with USB boot selection to support of USB Booting in my Custom Base Board?
Thanks,
Narasimma
@Narasimma Sure,If the same as STM32MP157C-DK2, There will be no problem.
Thank you @Baozhu,
Regards,
Narasimma