#include <Wire.h>
void setup() {
Serial.begin(115200);
while(!Serial);
Serial.println("I2C Scanner initialization");
Wire.begin();
Wire.setClock(100000UL);
Serial.println("I2C Scanner");
}
void loop() {
byte error, address;
int nDevices;
nDevices = 0;
Serial.println("I2C1 Scanning...");
for(address = 1; address < 127; address++) {
Wire.beginTransmission(address);
error = Wire.endTransmission();
if (error == 0) {
Serial.print("I2C1 device found at address 0x");
if (address < 16)
Serial.print("0");
Serial.println(address, HEX);
nDevices++;
}
else if (error == 4) {
Serial.print("Unknown error at address 0x");
if (address < 16)
Serial.print("0");
Serial.println(address, HEX);
}
}
if (nDevices == 0)
Serial.println("No I2C1 devices found");
else
Serial.println("I2C1 done");
Serial.println("");
delay(1000);
}
Try this sketch.