Power Pins
VIN - This is the power pin. To power the board, give it the same power as the logic level of your microcontroller - e.g. for a 3V microcontroller like a Feather M4, use 3V, or for a 5V microcontroller like Arduino, use 5V.
3Vo - This is the output from the onboard 3.3V regulator. If you have a need for a clean 3.3V output, you can use this! It can provide at least 100mA output.
GND - This is common ground for power and logic.
The 3Vo pin is a 3.3V output terminal. Connect 3.3V to the VIN pin.