Hercules 4WD Robot Controller

Yesterday i received the Skeletonbot_4WD Hercules kit. I assembled everything conform instructions.

-attached the motors
-attached a 7.4V lipu accu to j1
-attached a PC to j17
-uploaded the example software to the microcontroller

But the motors do nothing. They don’t move.
voltage at the motorconnectors. motor off=0Volt / motor on=0.02V -> NOT OK
voltage at J1 (battery connector) -> 7.6Volt -> OK

There is another (minor) problem with the board that i can repair. The powerled (PWR) is not properly soldered to the board. It does not work. I can make it work by connecting the led-lead to the underlaying pad where it should be connected to.

Can you give me advice how to solve the problems with the motorvoltage?

With friendly regards,

Rein

[size=150]Hi All
I have the same problem with my 4WD Robot Controller. But how you can make it work?
Can you show me where is the LED locations on the board[/size]

Thanks :wink:

The powerled and resetled are left and right of the reset button

Problem with the powerled is solved! It was a hardware problem on the print. My local Seeedstudio distributor (iprototype.nl) replaced the controller board and the powerled on the new controllerboard is working properly.

But…the motors are not running. In running state the motors receive 0.02Volt from the controller board. That is not good :frowning:
It seems that the Atmel Chip (Arduino) is working properly but the H-bridge (motordriver) does not work.
Does anybody know how i can fix this?

I found out that is is a software problem. The hardware is OK but the software example is not working with default controller from the kit.
I can get the motors running with digitalWrite(PINCS,HIGH) , but they are only running forward
Still trying to get better control by manipulating PINM1F, PINM1R, PINM2F, PINM2R but without success.

Suggestions are very welcome :wink:

Problem solved.

I made a new program (without the Seeedstrudio libraries) to test the robot. It is attached to this message



// order SEN
#define RETM1SPEED      0x87
#define RETM2SPEED      0x88
#define RETM1STATE      0x90
#define RETM2STATE      0x91

// motor state
#define STOP            0x00        // motor stop
#define RUN             0x01        // motor run

//motor direction
#define DIRF            0x00        // Forward
#define DIRR            0x01        // Reversion

// pin ctrl
#define PINCS           6           // all mos cs
#define PINM1F          4
#define PINM1R          5
#define PINM2F          7
#define PINM2R          8

int motorState;


void setup()
{
   //motorStop();
   Serial.begin(19200);
   Serial.println("HERCULES 4WD TEST");
   pinMode(PINCS, OUTPUT);
    pinMode(PINM1F, OUTPUT);
    pinMode(PINM1R, OUTPUT);
    pinMode(PINM2F, OUTPUT);
    pinMode(PINM2R, OUTPUT);
   motorStop(100);
}

void loop()
{
  motorForward(100); 
  motorStop(2000);
  motorReverse(100);
  motorStop(2000); 

}


void motorStop(int duration)
{
  Serial.println("stop");
  digitalWrite(PINCS,LOW);
  digitalWrite(PINM1R,LOW);
  digitalWrite(PINM1F,LOW);
  digitalWrite(PINM2F,LOW);
  digitalWrite(PINM2R,LOW);
  delay(duration);
 
}

void motorForward(int duration)
{
   Serial.println("forward");
   digitalWrite(PINM1R,HIGH);
   digitalWrite(PINM1F,LOW);
   digitalWrite(PINM2F,HIGH);
   digitalWrite(PINM2R,LOW);
   digitalWrite(PINCS,HIGH);
   delay(duration);
}

void motorReverse(int duration)
{
   Serial.println("reverse");
   digitalWrite(PINM1R,LOW);
   digitalWrite(PINM1F,HIGH);
   digitalWrite(PINM2F,LOW);
   digitalWrite(PINM2R,HIGH);
   digitalWrite(PINCS,HIGH);
   delay(duration);
}




//*****************************************************************************************************
// * END FILE
// *****************************************************************************************************

I am missing some things about the feedbacksensors in the Seeedstudio wiki (seeedstudio.com/wiki/Hercules_Du … Controller )

    • which type of sensor/ic is used?
    • how can i read a value from the sensors (serial/i2c/digital)?
    • where can i find the sensor datasheet?

The problem with the feedbacksensors is solved too. Now the device is 100% working.
I you want to know how i solved it, then look at the code. You can download the sourcecode at http://www.mechanicape.nl/hercules-4wd and http://www.mechanicape.nl/sites/default/files/hercules-131011a.zip

//MECHANICAPE.NL FIRMWARE FOR SEEEDSTUDIO HERCULES 4WD CONTROLLER
//Copyright By Rein Velt / http://mechanicape.nl        
//May be used under the terms and conditions of Create Commons CC-BY-SA
//=====================================================================
// The device is controlled by serial commands. The command is send 
// to the controllerboard. The controllerboard performs the 
// requested action and sends a response message
// back to the requestor.
// The commands, descriptions and responses are:
//  CMD     DESCRIPTION                     RESPONSE
//  M0      Motor OFF                      -returns M0,speedL,speedR\n
//  M1      Motor Forward                  -returns M1,speedL,speedR\n
//  M2      Motor Reverse                  -returns M2,speedL,speedR\n
//  M3      Motor Turn Left (ccw)          -returns M3,speedL,speedR\n
//  M4      Motor Turn Right (cw)          -returns M4,speedL,speedR\n
//  MT      Motor Test (test motors)       -returns MT,speedL,speedR\n
//  S0..S9  Speed (0=stop,.., 9=fast)      -returns S*,speedL,speedR\n
//  B?      Query battery voltage          -returns B?,millivolts\n
//
//  the comma is used to separate commands when more are following
//  the newline is used to terminate one or more commands
//  eg:
//      M1\n 
//      S5,M1,M1,S3,M2,M3,M0\n
//====================================================================

#include <avr/wdt.h>

// pin ctrl
#define PINRX           0           // receive serial data
#define PINTX           1           // send serial data
#define PININT0         2           // interrupt 0
#define PININT1         3           // interrupt 1
#define PINCS           6           // all motors cs
#define PINM1F          4           // motor 1 forward
#define PINM1R          5           // motor 1 reverse
#define PINM2F          7           // motor 2 forward
#define PINM2R          8           // motor 2 reverse
#define PINPWMA         9           // PWM channel A (motor A speed)
#define PINPWMB         10          // PWM channel B (motor B speed)
#define PINVS           A6          // voltage/battery sensor



//global vars
volatile int leftFeedback = 0;
volatile int rightFeedback = 0;
int motorSpeed=0;


void setup()
{
  //initialize pins (make them output) 
  pinMode(PINCS, OUTPUT);
  pinMode(PINM1F, OUTPUT);
  pinMode(PINM1R, OUTPUT);
  pinMode(PINM2F, OUTPUT);
  pinMode(PINM2R, OUTPUT);
  pinMode(PINVS,  INPUT);

  //initialize motors
  motorStop();

  //initialize interrupts
  attachInterrupt(0, leftInterruptHandler, CHANGE);
  attachInterrupt(1, rightInterruptHandler, CHANGE);

  //initialize serial port
  Serial.begin(19200);
  Serial.println("//MECHANIC APE HERCULES 4WD ROBOTFIRMWARE V1.0");
  Serial.print("//Battery=");
  Serial.print(getBatteryVoltage());
  Serial.print("mV");
  Serial.println();
  Serial.println("OK");

  //initialize watch dog timer and set it to 2 seconds
  wdt_enable(WDTO_2S);
}


void loop()
{
  wdt_reset();  //reset watch dog timer
  processSerialData(); //read data from serial and send it to the motors
  resetFeedback();  //reset speed sensors
}


//**** INTERRUPT HANDLER ******************************************************************************


void leftInterruptHandler()
{
  leftFeedback++;
}


void rightInterruptHandler()
{
  rightFeedback++;
}


void resetFeedback()
{
  leftFeedback=0;
  rightFeedback=0;
}


//**** MOTOR CONTROLLER *******************************************************************************


void motorSetSpeed(int power)
{
  motorSpeed=power;
  analogWrite(PINPWMA,motorSpeed);
  analogWrite(PINPWMB,motorSpeed);
}


void motorStop()
{
  digitalWrite(PINCS,LOW);
  digitalWrite(PINM1R,LOW);
  digitalWrite(PINM1F,LOW);
  digitalWrite(PINM2F,LOW);
  digitalWrite(PINM2R,LOW); 
}


void motorForward()
{
  digitalWrite(PINM1R,HIGH);
  digitalWrite(PINM1F,LOW);
  digitalWrite(PINM2F,HIGH);
  digitalWrite(PINM2R,LOW);
  digitalWrite(PINCS,HIGH);
}

void motorReverse()
{
  digitalWrite(PINM1R,LOW);
  digitalWrite(PINM1F,HIGH);
  digitalWrite(PINM2F,LOW);
  digitalWrite(PINM2R,HIGH);
  digitalWrite(PINCS,HIGH);
}


void motorTurnLeft()
{
  digitalWrite(PINM1R,LOW);
  digitalWrite(PINM1F,HIGH);
  digitalWrite(PINM2F,HIGH);
  digitalWrite(PINM2R,LOW);
  digitalWrite(PINCS,HIGH);
}


void motorTurnRight()
{
  digitalWrite(PINM1R,HIGH);
  digitalWrite(PINM1F,LOW);
  digitalWrite(PINM2F,LOW);
  digitalWrite(PINM2R,HIGH);
  digitalWrite(PINCS,HIGH);

}


//**** MESSAGE HANDLING ******************************************************************************


void processSerialData()
{
  if (Serial.available()>2)
  {
    int commandByte= Serial.read();
    int valueByte  = Serial.read();
    int endofline  = Serial.read();
    //a message has 3 bytes
    //this first byte is always M (Motor) or S (Speed)
    //the second byte is a number (0|1|2|3|4|..|9) 
    //the third byte is a comma or a newline (,|\n)
    
    
    //handle the motor request
    if (commandByte==77 && (endofline==10 || endofline==44)) //M
    {
      //incoming data is correct and conform specs  
      motorSetSpeed(motorSpeed);      
      switch (valueByte)
      {
        //control the motors
      case 48+0: 
        motorStop(); 
        break;       //M0\n
      case 48+1: 
        motorForward(); 
        break;      //M1\n
      case 48+2: 
        motorReverse(); 
        break;      //M2\n
      case 48+3: 
        motorTurnLeft(); 
        break;     //M3\n
      case 48+4: 
        motorTurnRight(); 
        break;     //M4\n
      case 84:
        motorTest(); //MT\n
        break;
      default: 
        motorStop();  
        break;    //fail safe
      } //end-switch

      //confirm the serial request by sending a response
      Serial.print(char(commandByte));
      Serial.print(char(valueByte));
      Serial.print(char(44));
      Serial.print(leftFeedback);
      Serial.print(char(44));
      Serial.print(rightFeedback);
      Serial.println();
    } 
  
    //handle the motorspeed request
    if (commandByte==83 && (endofline==10 || endofline==44)) //S
    {
      //incoming data is correct and conform specs        
      if (valueByte>47 && valueByte<59)
      { 
        //set the motorspeed
        int motorNewSpeed=(valueByte-48)*26;
        motorSetSpeed(motorNewSpeed);

      }
      //confirm the serial request by sending a response
      Serial.print(char(commandByte));
      Serial.println(char(valueByte));
    } 

    //handle the battery voltage request
    if (commandByte==66 && (endofline==10 || endofline==44)) //B
    {
      
      int millivolt=getBatteryVoltage();
      //confirm the serial request by sending a response
      Serial.print(char(commandByte));
      Serial.print(char(valueByte));
      Serial.print(char(44));
      Serial.print(millivolt);
      Serial.println();
    } 

  }
  else
  {
    //no data
    motorStop();  //fail safe

  }
  delay(100); //this delay can be tweaked or omitted to adjust accuracy. keep it low!
}



//***** SENSOR HANDLING ******************************************************************************

int getBatteryVoltage()
{

  int value=analogRead(PINVS);
  int millivolt=round((float)(value)/0.037479); //guess
  return millivolt;
}
//***** SYSTEM TEST **********************************************************************************

void motorTest()
{
  for (int i=0;i<255;i++)
  {
    wdt_reset();
    motorSetSpeed(i);
    motorTurnRight();
    delay(50) ;
  }
  for (int i=255;i>-1;i--)
  {
    wdt_reset();
    motorSetSpeed(i);
    motorTurnRight();
    delay(50) ;
  }
  motorStop();
}
//*****************************************************************************************************
// * END FILE
// *****************************************************************************************************



hello