ArnieO
March 17, 2021, 8:30pm
1
I am trying to connect to LoRaWAN by following the instructions on the Wiki , but no success so far.
The response to AT+JOIN is:
+JOIN: Start
+JOIN: NORMAL
I also tried AT+JOIN=DR3 (which should be what I am using). The response is:
+JOIN: Start
+JOIN: NORMAL
+JOIN: Join failed
+JOIN: Done
Anyone?
ArnieO
March 18, 2021, 3:18pm
2
Update:
I am finally able to connect using ABP authentication, not OTAA.
This might be due to shortcomings in my DIY single-channel gateway.
Don’t use a single-channel gateway. They are essentially non-compliant with LoRaWan. Modestly-priced, compliant, 8-channel gateways are available. https://www.thethingsnetwork.org/docs/gateways/start/single-channel.html
ArnieO
March 23, 2021, 7:22am
4
Don’t use a single-channel gateway. They are essentially non-compliant with LoRaWan. Modestly-priced, compliant, 8-channel gateways are available. https://www.thethingsnetwork.org/docs/gateways/start/single-channel.html
That is surely good advise! It is for the moment a cost/benefit issue for me to work with this simplified gateway, in addition to getting learning points like this one - that improve my understanding of LoRa.
PS: I have been able to confirm the GW firmware was the problem.
ma-iot
June 29, 2021, 5:33pm
5
I’m using full gateway and cannot AT+JOIN TheThingsNetwork with the LoRa-E5 module (FW version 4.0.11) in OTAA mode.
TheThingsNetwork sees the Join request and rejects it due to “MIC mismatch” according to TheThingsNetwork.
So, it seems that the LoRa-E5 is not calculating the MIC properly?
This is confirmed by the packet decoder at https://lorawan-packet-decoder-0ta6puiniaut.runkit.sh/
The raw packet is from TTN Application Console:
Assuming hex-encoded packet
0006000000000000800203902420F1F72CD9C9589BF71A
Message Type = Join Request
PHYPayload = 0006000000000000800203902420F1F72CD9C9589BF71A
( PHYPayload = MHDR[1] | MACPayload[..] | MIC[4] )
MHDR = 00
MACPayload = 06000000000000800203902420F1F72CD9C9
MIC = 589BF71A (from packet) INVALID (tried MSB 0000-FFFF)
= 4E25A4D0 (expected, assuming 32 bits frame counter with MSB 0000)
( MACPayload = AppEUI[8] | DevEUI[8] | DevNonce[2] )
AppEUI = 8000000000000006
DevEUI = 2CF7F12024900302
DevNonce = C9D9
Has anyone been able to make OTAA work?