"Guru Meditation Error" ESP32S3 Sense with Round Display

I just followed the tutorial in Get Started With Round Display

From Step1 to Step5
And after I uploaded the “HardwareTest.ino” to my board
The serial Monitor showed this error, and the display didn’t show anything.

Error Message:

XIAO round screen - LVGL_Arduino
Guru Meditation Error: Core  1 panic'ed (StoreProhibited). Exception was unhandled.

Core  1 register dump:
PC      : 0x42026816  PS      : 0x00060830  A0      : 0x820268ec  A1      : 0x3fcebe30  
A2      : 0x00000010  A3      : 0x00000001  A4      : 0x60004000  A5      : 0x00000009  
A6      : 0x000000ff  A7      : 0x00000000  A8      : 0x08000000  A9      : 0x3fcebe00  
A10     : 0x3fca3698  A11     : 0x00000001  A12     : 0x02625a00  A13     : 0xffffffff  
A14     : 0x00000031  A15     : 0x00000000  SAR     : 0x0000001c  EXCCAUSE: 0x0000001d  
EXCVADDR: 0x00000010  LBEG    : 0x4202cc18  LEND    : 0x4202cc5f  LCOUNT  : 0x00000003  


Backtrace: 0x42026813:0x3fcebe30 0x420268e9:0x3fcebe60 0x420268f4:0x3fcebe80 0x42001fcb:0x3fcebea0 0x42001fe7:0x3fcebec0 0x42002303:0x3fcebee0 0x4202d7da:0x3fcebf00 0x4037e0b6:0x3fcebf20

ELF file SHA256: 8d26448727f8f7da

Rebooting...
ESP-ROM:esp32s3-20210327
Build:Mar 27 2021
rst:0xc (RTC_SW_CPU_RST),boot:0x28 (SPI_FAST_FLASH_BOOT)
Saved PC:0x403791c6
SPIWP:0xee
mode:DIO, clock div:1
load:0x3fce3818,len:0x508
load:0x403c9700,len:0x4
load:0x403c9704,len:0xad0
load:0x403cc700,len:0x29e4
entry 0x403c9880

Here’s the code:

#include <lvgl.h>

// uncomment a library for display driver
#define USE_TFT_ESPI_LIBRARY
// #define USE_ARDUINO_GFX_LIBRARY

#include "lv_xiao_round_screen.h"
#include "lv_hardware_test.h"

void setup()
{
    Serial.begin( 115200 );  //prepare for possible serial debug 
    Serial.println( "XIAO round screen - LVGL_Arduino" );

    lv_init();

    lv_xiao_disp_init();
    lv_xiao_touch_init();

    lv_hardware_test();
}

void loop()
{
    lv_timer_handler();  //let the GUI do its work 
    delay( 5 );
}

Thank you!

Hi there,
Looks like the BSP is not correct, Do you know which BSP you are using?
Roll it back to the 2.0.11 and try again.
HTH
GL :slight_smile: PJ
:v:

Thanks a lot!
I went to “Tools” >> “Board” >> “Board Manager”
,and changed the “esp32” version from 3.0.3 to 2.0.11
It worked!
Thank you so much. :wink: