The battery connector on the Grove - Xbee Carrier V1.0 is incompatible with the Lipo 2A (POW 1032C 1P). The battery connector on the CUI32Stem is also incompatible with the Lipo connector. Can I get an adapter to connect the Lipo to these devices?
You can see here,
http://www.seeedstudio.com/wiki/index.php?title=Bee_Stem#Hardware_Installation
Check that the red matching ‘+’ , black matching ‘-’ ;
Check this:
seeedstudio.com/depot/jst-25 … th=178_179