Is Grove - WS2813 RGB LED Strip Waterproof - 60 LED/m - 1m SKU 104020109 works with Seeeduino Lotus Cortex-M0+ SKU 102010228? It’s IO Input Voltage is 3.3V
Hi there~
The led strip max current is 3.6A per meter / 0.06A per LED. You can use the Seeeduino Lotus Cortex-M0+ to control the signal, GND. You can connect the external power supply(5V+GND) to led strip. thanks.