Grove vision AI2 Lighting

Does anyone have thoughts on how I can trigger lighting for images from the grove vision AI 2?

Does anyone know if I can programatically fix the exposure of the camera, or if it is using autoexposure (is this a camera ‘feature’ I can turn off?)

I have a project that will be looking at small things that are moving, so I need to swap out the base camera for one with a close up lense, and some strobed lighting so things are not blurred.

Any ideas? Do I just need to dig in and read the SDK docs? Is this possible?

Thanks,
Luc

So… I found the strobe output exists from the camera module on some variants… Doesn’t look to be there in the version supplied with the vision ai2 board…

Need to build a level shifter and such, but it looks doable on paper so far.