Grove Vision AI V2 - Save Image to SD CARD

@PJ_Glasso I have a RAK 3172 (STM32WL uP) successfully operating the WE2 via commands via I2C communications, running a model and returning results. The WE2 contains SSCMA-Micro. I’ve referred to SSCMA-Micro GitHub at_protocol, but have yet to be able to cause an image to be stored to the SD CARD. Note, I am not using the Arduino based SSCMA library (as it does not currently support the SMT32 family). I have tried various iterations of AT+SAMPLE and AT+TRIGGER and AT+INVOKE (which can send images files via a serial link).
Do you have any guidance on command(s) needed to have the SSCMA-MICRO firmware store an image file to the on-board SD Card?
Thanks in advance!

Hi there,

So I have NOT tried this Myself but AFAIK it works,
SSCMA-Micro does support saving JPEGs to the module’s SD card, but it’s not done with AT+SAMPLE / AT+TRIGGER / AT+INVOKE by themselves.

On Grove Vision AI V2 (WE2 + SSCMA-Micro), SD saving is driven by an “action trigger”:

The command you want

AT+ACTION="save_jpeg()"\r

Set the action once:
Seeed’s docs explicitly say that calling save_jpeg() sends AT+ACTION="save_jpeg()", and it “should only be called once.”

Then: every INVOKE will save a JPEG

After the action is set, each time you invoke (i.e., run the pipeline), the module will save a JPEG to the SD card. The Seeed example literally does: AI.save_jpeg(); once in setup, then AI.invoke(...) repeatedly, and “each invoke saves JPEG.”

So from your STM32WL/RAK3172 side, the flow is:

  1. Once at startup:
AT+ACTION="save_jpeg()"\r
  1. hen repeatedly (whatever your normal run command is):
  • AT+INVOKE... (or the equivalent you’re already using successfully)

To stop saving (important)

You must clear the action set (even after reboot, per the docs):crossed_fingers:

AT+ACTION=""\r

Seeed notes this is equivalent to clean_actions() and must be done if you no longer want JPEGs stored.

SD card “gotchas” that matter

If they still don’t see files:

  • SD must be FAT32 (with 8192 cluster size) or exFAT (Seeed recommendation).
  • Firmware needs to be new enough (Seeed calls out later than 2024-04-18).
  • Files go under a default export folder; the system creates session subfolders and tracks the latest folder in a hidden .sscma file (don’t edit it).

Those are about capturing/streaming/returning images (e.g., base64 over UART) — they don’t automatically configure the “save-to-SD” action. The SD write is specifically tied to the ACTION trigger mechanism.

HTH
GL :slight_smile: PJ :v:

Time permitting I’ll check it out, as I do have a use case for it. :+1:

@PJ_Glasso I will test with the guidance you have provided.

Please share the link to the Seeed’s doc you mention and the Seeed example that uses the AI.save_jpeg();. I went through the Wiki again and the GitHUb of SSCMA-Micro but did not come across it?

Additional comments. I was able to implement the AT+ACTION both to start saving to the SD CARD and to stop it, as you suggest, hooray!

However, the images are low resolution (~3KB). Is there a way to save the full resolution image sense by the OV5647 camera?
Thanks!

Jim M

Hi there,

So, this would be that :grin:

Example 3.

I would think you can set the default to be Higher maybe.

HTH
GL :slight_smile: PJ :v:

The command you need is AT+ACTION="save_jpeg()", followed by your standard AT+INVOKE command. This is not done with AT+SAMPLE or AT+TRIGGER alone .

The key is that the SSCMA-Micro firmware on your WE2 uses an “action trigger” system for SD card saving. You set the action once, and then every subsequent inference will save an image.

That explains why just using AT+SAMPLE or AT+TRIGGER alone wasn’t working. Those commands probably just handle the inference part without knowing you wanted the image saved. The action command acts like a configuration that tells the firmware what to do with each inference result.

So the workflow would be something like. First send AT+ACTION with the save command to set the behavior. Then your normal AT+INVOKE commands will both process the image and save it to SD. That way you don’t have to specify the save every single time, which is smart for continuous operation.