I bought the Grove-Temperature Sensor V1.2 and connected to M5StickC (https://m5stack.com/products/stick-c). I copied almost all the code from the specs page to convert the analog read to actual temperature, only adding the #include <M5StickC.h> and the M5.begin, but the temperature is way off and very oscillating. I am using pin 32 to read the data, Is it correct? Is it a sensor issue?
I solved the issue, I am getting the correct temperature now.
I changed the code to:
#include <M5StickC.h> #include <math.h>
const int B = 4275;
const float R0 = 100000;
const int PIN = 33;
void setup() {
M5.begin();
Serial.begin(115200);
}
void loop() {
int a = analogRead(PIN);
float R = 4095.0/a-1.0;
R = R0*R;
float temperature = 1.0 / (log(R / R0) / B + 1 / 298.15) - 273.15;
Serial.println(temperature);
delay(500);
}
The correct pin was 33, and modified the 1023.0 to 4095.0 in the formula because esp32 is returning values between 0 and 4096. But anyway, the temperature readings were too high. Then, I modified the grove cable (as is explained here https://tinkerfarm.net/projects/the-m5stickc/the-5-volt-danger-with-the-m5stickc/) feeding the temperature sensor with 3.3v instead of 5v. And, now, (with no additional code changes) the temperature is correct.