Grove Shield for Wio Lite - with AdaFruit Feather - not recognizing port

Hi,
I am using these 2 together:



When plugging only the feather the port appears and I can upload coad etc…
When putting it inside the shield, the charge led blinks rapidly and is not able to recognize the port at all.
Is this board not compatible? if not, is there any workaround for this?
I tried with all shields states(5V,Battery powered, middle one).
Thanks.

We haven’t tested it.But in theory it should be compatible.

It doesn’t recognize the board when connected to the shield, is there anything that can be done?

Problem solved, the shield has GND where the enable pin is, meaning disabling the board once connected. to solve this I didn’t connect the en pin to the shield, and can see the board.