Hi, i figure out with some help stackoverflow.com/questions/2483 … ed-display
This is my version now of the library, used to load 16x16 font. It still not much faster enough.
[code]void SeeedGrayOLED::putChar(unsigned char C)
{
if(C < 32 || C > 127) //Ignore non-printable ASCII characters. This can be modified for multilingual font.
{
C=’ '; //Space
}
char c,byte = 0x00;
volatile unsigned char nibble_lookup[] = { 0, grayL, grayH, grayH | grayL };
for(int ii=0;ii<2;ii++){
for(int i=0;i<8;i++)
{
for(int j=0;j<32;j+=2)
{
byte = pgm_read_byte(&hallfetica_normal[C-32][j+ii]);
c = nibble_lookup[(byte >> (8-i)) & 3];
sendData(c);
}
}
}
}[/code]
And this the font loaded
uint8_t hallfetica_normal[][32] PROGMEM={
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // <space>
{0x00,0x00,0x00,0x00,0x00,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x00,0x00,0x00,0x00,0x03,0x00,0x00,0x00,0x00,0x00}, // !
{0x00,0x00,0x00,0x00,0x00,0x00,0x03,0x60,0x03,0x60,0x03,0x60,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // "
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x06,0xC0,0x06,0xC0,0x1F,0xE0,0x06,0xC0,0x06,0xC0,0x1F,0xE0,0x06,0xC0,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // #
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x07,0xF8,0x0D,0x80,0x0D,0x80,0x0F,0xE0,0x07,0xF0,0x01,0xB0,0x01,0xB0,0x07,0xF0,0x0F,0xE0,0x01,0x80,0x00,0x00,0x00,0x00}, // $
{0x00,0x00,0x00,0x00,0x3C,0x18,0x66,0x30,0x66,0x60,0x66,0x60,0x66,0xC0,0x3D,0x80,0x01,0xBC,0x03,0x66,0x06,0x66,0x06,0x66,0x0C,0x66,0x18,0x3C,0x00,0x00,0x00,0x00}, // %
{0x00,0x00,0x00,0x00,0x07,0x80,0x0F,0xC0,0x0C,0xC0,0x0C,0xC0,0x07,0x80,0x07,0x98,0x0D,0x98,0x18,0xD8,0x18,0xF0,0x1C,0x70,0x0F,0xF8,0x07,0x98,0x00,0x00,0x00,0x00}, // &
{0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // '
{0x00,0x00,0x00,0x00,0x00,0xC0,0x01,0x80,0x01,0x80,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x01,0x80,0x01,0x80,0x00,0xC0,0x00,0x00,0x00,0x00,0x00,0x00}, // (
{0x00,0x00,0x00,0x00,0x0C,0x00,0x06,0x00,0x06,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x06,0x00,0x06,0x00,0x0C,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // )
{0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0xC0,0x1F,0xDC,0x1F,0xFC,0x0F,0xFC,0x03,0xF0,0x0F,0xF8,0x07,0x38,0x02,0x10,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // *
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x01,0x80,0x0F,0xF0,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00}, // +
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x00,0x80,0x01,0x00,0x00,0x00,0x00,0x00}, // ,
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xE0,0x0F,0xE0,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // -
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00}, // .
{0x00,0x00,0x00,0x00,0x00,0x18,0x00,0x30,0x00,0x30,0x00,0x60,0x00,0x60,0x00,0xC0,0x00,0xC0,0x01,0x80,0x01,0x80,0x03,0x00,0x03,0x00,0x06,0x00,0x00,0x00,0x00,0x00}, // /
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x0E,0x38,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0E,0x38,0x07,0xF0,0x00,0x00,0x00,0x00}, // 0
{0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00}, // 1
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x07,0xF0,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xF8,0x00,0x00,0x00,0x00}, // 2
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x07,0xF8,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // 3
{0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x60,0x0C,0x60,0x07,0xF8,0x00,0x60,0x00,0x60,0x00,0x60,0x00,0x60,0x00,0x00,0x00,0x00}, // 4
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xF0,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // 5
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xF8,0x0E,0x1C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0E,0x1C,0x07,0xF0,0x00,0x00,0x00,0x00}, // 6
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF8,0x00,0x30,0x00,0x30,0x00,0x60,0x00,0x60,0x00,0xC0,0x00,0xC0,0x01,0x80,0x01,0x80,0x03,0x00,0x03,0x00,0x00,0x00,0x00,0x00}, // 7
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x07,0xF8,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x07,0xF0,0x00,0x00,0x00,0x00}, // 8
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x0E,0x1C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0E,0x1C,0x03,0xFC,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x07,0xF8,0x00,0x00,0x00,0x00}, // 9
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // :
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x00,0x80,0x01,0x00,0x00,0x00,0x00,0x00}, // ;
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x30,0x00,0xE0,0x03,0x80,0x07,0x00,0x07,0x00,0x03,0x80,0x00,0xE0,0x00,0x30,0x00,0x00,0x00,0x00,0x00,0x00}, // <
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF8,0x00,0x00,0x00,0x00,0x0F,0xF8,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // =
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x03,0x00,0x01,0xC0,0x00,0xE0,0x00,0x38,0x00,0x38,0x00,0xE0,0x01,0xC0,0x03,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // >
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x00,0x18,0x00,0x18,0x00,0x18,0x01,0xF0,0x03,0x00,0x03,0x00,0x03,0x00,0x00,0x00,0x00,0x00,0x03,0x00,0x00,0x00,0x00,0x00}, // ?
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x08,0x08,0x09,0xE8,0x0A,0x28,0x0A,0x28,0x0A,0x28,0x0A,0x28,0x09,0xF8,0x08,0x00,0x07,0xF8,0x00,0x00,0x00,0x00,0x00,0x00}, // @
{0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x03,0xC0,0x03,0xC0,0x03,0xC0,0x06,0x60,0x06,0x60,0x07,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x18,0x18,0x00,0x00,0x00,0x00}, // A
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0F,0xF8,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // B
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x07,0xF8,0x00,0x00,0x00,0x00}, // C
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // D
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x07,0xF8,0x00,0x00,0x00,0x00}, // E
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x00,0x00,0x00,0x00}, // F
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xFC,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0xFC,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x07,0xFC,0x00,0x00,0x00,0x00}, // G
{0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0F,0xFC,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x00,0x00,0x00,0x00}, // H
{0x00,0x00,0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00}, // I
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // J
{0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x18,0x0C,0x38,0x0C,0x30,0x0C,0x60,0x0C,0xE0,0x0F,0xF0,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x00,0x00,0x00,0x00}, // K
{0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x07,0xF8,0x00,0x00,0x00,0x00}, // L
{0x00,0x00,0x00,0x00,0x00,0x00,0x7F,0xFC,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x61,0x86,0x00,0x00,0x00,0x00}, // M
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF8,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x0C,0x00,0x00,0x00,0x00}, // N
{0x00,0x00,0x00,0x00,0x00,0x00,0x03,0xFC,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x03,0xFC,0x00,0x00,0x00,0x00}, // O
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0F,0xF0,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x00,0x00,0x00,0x00}, // P
{0x00,0x00,0x00,0x00,0x03,0xFC,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x06,0x03,0xFC,0x00,0x60,0x00,0x70,0x00,0x3E}, // Q
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xF0,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0F,0xF8,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x0C,0x18,0x00,0x00,0x00,0x00}, // R
{0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x07,0xF0,0x00,0x18,0x00,0x18,0x00,0x18,0x00,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // S
{0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xFC,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0x00,0x00,0x00}, // T
{0x00,0x00,0x00,0x00,0x00,0x00,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x18,0x0F,0xF0,0x00,0x00,0x00,0x00}, // U
{0x00,0x00,0x00,0x00,0x00,0x00,0x18,0x18,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x06,0x60,0x06,0x60,0x06,0x60,0x03,0xC0,0x03,0xC0,0x03,0xC0,0x01,0x80,0x00,0x00,0x00,0x00}, // V
{0x00,0x00,0x00,0x00,0x00,0x00,0x21,0x84,0x23,0x8C,0x33,0x8C,0x33,0xD8,0x36,0xD8,0x36,0xD8,0x1E,0xD8,0x1E,0x70,0x1C,0x70,0x1C,0x70,0x0C,0x70,0x00,0x00,0x00,0x00}, // W
{0x00,0x00,0x00,0x00,0x00,0x00,0x1C,0x38,0x0C,0x30,0x06,0x60,0x07,0xE0,0x03,0xC0,0x01,0x80,0x03,0xC0,0x06,0x60,0x06,0x60,0x0C,0x30,0x1C,0x38,0x00,0x00,0x00,0x00}, // X
{0x00,0x00,0x00,0x00,0x00,0x00,0x1C,0x38,0x0C,0x30,0x06,0x60,0x07,0xE0,0x03,0xC0,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00}, // Y
{0x00,0x00,0x00,0x00,0x00,0x00,0x1F,0xF0,0x00,0x60,0x00,0x60,0x00,0xC0,0x01,0x80,0x01,0x80,0x03,0x00,0x06,0x00,0x06,0x00,0x0C,0x00,0x1F,0xF8,0x00,0x00,0x00,0x00}, // Z
{0x00,0x00,0x03,0xE0,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0xE0,0x03,0xE0,0x00,0x00}, // [
{0x00,0x00,0x00,0x00,0x0C,0x00,0x06,0x00,0x07,0x00,0x07,0x00,0x03,0x80,0x03,0x80,0x01,0xC0,0x01,0xC0,0x00,0xC0,0x00,0xE0,0x00,0x60,0x00,0x70,0x00,0x30,0x00,0x00}, // <backslash>
{0x00,0x00,0x03,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x03,0xC0,0x03,0xC0,0x00,0x00}, // ]
{0x00,0x00,0x00,0x00,0x01,0xC0,0x03,0xE0,0x07,0x60,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // ^
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0xFF,0xFF,0x00,0x00}, // _
{0x00,0x00,0x00,0x00,0x03,0xE0,0x06,0x30,0x06,0x30,0x06,0x30,0x03,0xE0,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // `
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xE0,0x00,0x30,0x00,0x30,0x07,0xF0,0x0E,0x30,0x0C,0x30,0x0E,0x30,0x07,0xF0,0x00,0x00,0x00,0x00,0x00,0x00}, // a
{0x00,0x00,0x00,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0F,0xE0,0x00,0x00,0x00,0x00,0x00,0x00}, // b
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x07,0xF0,0x00,0x00,0x00,0x00,0x00,0x00}, // c
{0x00,0x00,0x00,0x00,0x00,0x30,0x00,0x30,0x00,0x30,0x07,0xF0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x07,0xF0,0x00,0x00,0x00,0x00,0x00,0x00}, // d
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x0C,0x00,0x0C,0x00,0x0F,0xF0,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x07,0xF0,0x00,0x00,0x00,0x00,0x00,0x00}, // e
{0x00,0x00,0x00,0x00,0x03,0xE0,0x06,0x00,0x06,0x00,0x0F,0xC0,0x06,0x00,0x06,0x00,0x06,0x00,0x06,0x00,0x06,0x00,0x06,0x00,0x06,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // f
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xE0,0x18,0x60,0x18,0x60,0x18,0x60,0x18,0x60,0x18,0x60,0x18,0x60,0x0F,0xE0,0x00,0x60,0x00,0x60,0x0F,0xC0,0x00,0x00}, // g
{0x00,0x00,0x00,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0F,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x00,0x00,0x00,0x00,0x00,0x00}, // h
{0x00,0x00,0x00,0x00,0x00,0x00,0x03,0x00,0x00,0x00,0x01,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // i
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0xC0,0x00,0x00,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x03,0xC0,0x07,0x80,0x00,0x00}, // j
{0x00,0x00,0x00,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x30,0x0C,0x60,0x0C,0xC0,0x0F,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x00,0x00,0x00,0x00,0x00,0x00}, // k
{0x00,0x00,0x00,0x00,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x00,0x00,0x00,0x00,0x00,0x00}, // l
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x3F,0xF8,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x00,0x00,0x00,0x00,0x00,0x00}, // m
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x00,0x00,0x00,0x00,0x00,0x00}, // n
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x07,0xE0,0x00,0x00,0x00,0x00,0x00,0x00}, // o
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0F,0xE0,0x0C,0x00,0x0C,0x00,0x0C,0x00}, // p
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x07,0xF0,0x00,0x30,0x00,0x30,0x00,0x30}, // q
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0xE0,0x0C,0x30,0x0C,0x30,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x0C,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, // r
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF0,0x0C,0x00,0x0C,0x00,0x07,0xE0,0x00,0x30,0x00,0x30,0x00,0x30,0x0F,0xE0,0x00,0x00,0x00,0x00,0x00,0x00}, // s
{0x00,0x00,0x00,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x07,0xE0,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x03,0x00,0x01,0xF0,0x00,0x00,0x00,0x00,0x00,0x00}, // t
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x07,0xF0,0x00,0x00,0x00,0x00,0x00,0x00}, // u
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x18,0x06,0x30,0x06,0x30,0x06,0x60,0x03,0x60,0x03,0x60,0x01,0xC0,0x01,0xC0,0x00,0x00,0x00,0x00,0x00,0x00}, // v
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x31,0x8C,0x1F,0xFC,0x00,0x00,0x00,0x00,0x00,0x00}, // w
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0E,0x30,0x06,0x70,0x03,0x60,0x01,0xC0,0x01,0xC0,0x03,0xC0,0x03,0x60,0x06,0x30,0x00,0x00,0x00,0x00,0x00,0x00}, // x
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x0C,0x30,0x07,0xF0,0x00,0x30,0x00,0x30,0x0F,0xE0}, // y
{0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x07,0xF8,0x00,0x30,0x00,0x60,0x00,0xC0,0x00,0xC0,0x01,0x80,0x03,0x00,0x07,0xFC,0x00,0x00,0x00,0x00,0x00,0x00}, // z
{0x00,0x00,0x03,0xC0,0x03,0x00,0x02,0x00,0x02,0x00,0x02,0x00,0x02,0x00,0x06,0x00,0x06,0x00,0x02,0x00,0x02,0x00,0x02,0x00,0x03,0x00,0x03,0xC0,0x01,0xC0,0x00,0x00}, // {
{0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x01,0x80,0x00,0x00}, // |
{0x00,0x00,0x03,0xC0,0x01,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x00,0xE0,0x00,0x60,0x00,0xE0,0x00,0xC0,0x00,0xC0,0x00,0xC0,0x01,0xC0,0x01,0xC0,0x03,0x80,0x00,0x00}, // }
{0x00,0x00,0x00,0x00,0x07,0x80,0x0C,0xCC,0x0C,0xDC,0x00,0x78,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00} // ~
};