I would like to use two of the Grove MCP9600 sensors on the same I2C bus (I’m using a Lotus v1.1). I know that the two sensors will have the same addresses and that I need to change one of them. I see in the wiki where the address contacts are but I am not sure how I should alter them to have one of the sensors be on the alternate address.
Also, once this change has been made, what initialization changes are needed to then use two sets of functions throughout my code (i.e., get_temperature1() and get_temperature2())
Thanks for any help you can offer!
~JRG