Grove - Magnetic Sensor (AS5600) debug python file

Hi everyone,

I’m using the Grove - 12-bit Magnetic Rotary Position Sensor / Encoder (AS5600) to acquire some information on a wheel. I’m using python and a Raspberry Pi to acquire the data.

I’m very satisfied of the precision of the sensor, but I post on the forum because I have small errors when I move slowly my wheel like you can see on the attachments


.

I have some difficulties to debug my program because I cannot visualize properly due to the speed of the process (the error is on the convert_deltaAngleDeg_rotations function).

Do you have any suggestion to fix this issue or improve my program ?

from smbus import SMBus
import logging
from math import pi
import time
from dataclasses import dataclass
from numpy import deg2rad
import threading

logging.basicConfig(level=logging.INFO)

RADIUS_WHEEL = 0.04 # in meter

wait = threading.Event().wait

@dataclass
class Angle:
    rawValue: int
    degree: float
    radian: float
class single_encoder:
    def __init__(self, busI2C):
        self.bus = SMBus(busI2C) # Create an instance of the SMBus class
        self.AS5600_ADDRESS = 0x36 # I2C address of the AS5600 sensor
        self.AS5600_REG_ANGLE = 0x0E # Register to read the angular position
        self.rotations = 0
        self.totalDistance = 0
        self.rotationPerMinute = 0
        self.speed_dps = 0
        self.speed_rad_sec = 0
        self.linear_speed = 0

    def getRawAngle(self):
        """Reading data from the angle register
            
        Returns:
            rawAngle: Numeric value between 0 and 4096 representing the angle
        """
        data = self.bus.read_i2c_block_data(self.AS5600_ADDRESS, self.AS5600_REG_ANGLE, 2)
        rawAngle = ((data[0] & 0xFF) << 8 | (data[1] & 0xFF))
        return rawAngle
    
    def getDegree(self):
        """Convert raw data from the encoder to degree

        Returns:
            float: value in degree
        """
        rawAngle = self.getRawAngle()
        angleDegree = rawAngle / 4096 * 360.0
        return angleDegree
    
    def getRadian(self):
        """Convert raw data from the encoder to radian

        Returns:
            float: value in radian
        """
        rawAngle = self.getRawAngle()
        angleRadian = rawAngle / 4096 * 2 * pi
        return angleRadian
    
    def convert_deltaAngleDeg_rotations(delta_angle_deg):
        """Convertis la différence d'angle en rotation de roue
        
        Args:
            delta_angle_deg : différence d'angle en degrée
        """
        # ToDo : Measurement error (rotation) on low translation / move of the wheel
        if delta_angle_deg != 0:  # Detection of a move
            if abs(delta_angle_deg) >= 180: # we have crossed the 0°. The count of degree we moved is calculated by adding or subtracting a full turn (360°) depending on current sense of rotation
                if delta_angle_deg > 0: # the difference sign is positive we have moved clockwise (increment angle)
                    return (delta_angle_deg + 360) / 360
                else: # the difference sign is negative we have moved counter clockwise (decrement angle)
                    return (delta_angle_deg - 360) / 360
            else:
                return delta_angle_deg / 360
        else:
            return 0
        
    
    def calculate_rotationPerMinute(time_interval, rotations):
        return rotations / time_interval * 60

    def getSpeedDps(time_interval, delta_angle_deg):
        return delta_angle_deg / time_interval

    def getSpeedRadS(speed_dps):
        return deg2rad(speed_dps)

    def getLinearSpeed(speed_rad_sec):
        return RADIUS_WHEEL * speed_rad_sec

    def getDistance(totalAngleRad):
        return RADIUS_WHEEL * totalAngleRad
    
    def CalculateSpeed(self):
        """Process & update the speed variables of the object
        """
        last_time = time.time()
        last_angle = Angle(self.getRawAngle(), self.getDegree(), self.getRadian())
        while True:
            current_angle = Angle(self.getRawAngle(), self.getDegree(), self.getRadian())
            delta_angle_deg = round(current_angle.degree - last_angle.degree, 2)
            self.rotations += single_encoder.convert_deltaAngleDeg_rotations(delta_angle_deg)        
            current_time = time.time()
            delta_time = current_time - last_time
            logging.debug(f"delta_time = {delta_time}")
            if delta_time >= 1:  # update speed info every second
                self.rotationPerMinute = single_encoder.calculate_rotationPerMinute(delta_time, self.rotations)
                totalAngleDeg = self.rotations * 360
                totalAngleRad = deg2rad(totalAngleDeg)
                self.speed_dps = single_encoder.getSpeedDps(delta_time, totalAngleDeg)
                self.speed_rad_sec = single_encoder.getSpeedRadS(self.speed_dps)
                self.linear_speed = single_encoder.getLinearSpeed(self.speed_rad_sec)
                self.totalDistance += single_encoder.getDistance(totalAngleRad)    
                last_time = current_time
                self.rotations = 0
            last_angle = current_angle
    
    def Capture(self):
        Thread = threading.Thread(target=self.CalculateSpeed,daemon=True)
        Thread.start()
    
LeftEncoder = single_encoder(5)
LeftEncoder.Capture()
while True:
    print(f"number of rotations: {LeftEncoder.rotations}")
    wait(0.1)

Thanks in advance for your answer,
Best regards

Hi there,
What about using a filter?
Like with an IMU data , we use a filter to normalize the data? like Kalman Filter?
My .02
HTH
GL :slight_smile: PJ

Thanks, @PJ_Glasso for your answer,

Using a filter is my most valuable option at the moment.
I just wanted to ask if someone see an evident fix in my algorithm.

I’m still a newbie to apply filters for real-time applications….
A Kalman filter will probably have better performance, but a low-pass filter could also work, no?
I will try both.

Hi there,
YES… Low-pass for most, the Kalman to get a YAW and/or Tilt reading and more stable X,Y,Z :+1:
GL :slight_smile: PJ