Hi, so i just bought a Grove - GPS (Air530), but the module is not connecting to anything, it displays the following data in ublox and arduino serial monitor:
??:??:?? $GNZDA,,,,,,*56 ??:??:?? $GPTXT,01,01,01,ANTENNA OK*35 ??:??:?? $GNGGA,,,,,,0,00,25.5,,,,,,*64 ??:??:?? $GNGLL,,,,,,V,N*7A ??:??:?? $GNGSA,A,1,,,,,,,,,,,,,25.5,25.5,25.5,1*01 ??:??:?? $GNGSA,A,1,,,,,,,,,,,,,25.5,25.5,25.5,4*04 ??:??:?? $GPGSV,1,1,00,0*65 ??:??:?? $BDGSV,1,1,00,0*74 ??:??:?? $GNRMC,,V,,,,,,,,,,N,V*37 ??:??:?? $GNVTG,,,,,,,,,N*2E
I followed the tutorial of the wiki and clearly is not working. I have no idea about GPS, so any help its apreciated.